Other Parts Discussed in Thread: TPS65720 , BQ27421-G1 Hi,
CAn any one let me know how to shut down the TPS65720 once it is turned on once the PB_IN is pressed and both DCDC and LDO are turned on by setting the hold bits through I2C.
As there is no Key…
Other Parts Discussed in Thread: TPS65720 , TPS65721 hi,
I am working with tps65720/1 EVM modules. As a system designer i am trying to test its efficiency and compare with each other. I need help in the following topics:
1.SMPS
a) how will PWM/PFM mode…
Other Parts Discussed in Thread: TPS65720 hi
in the document given with tps65720 it says that an interrupt is cleared(after generation) when it is read, but when i use the GUI given with EVM board whenever the interrupt is generated it is erased in a second…
Part Number: TPS65720TPS65720_1EVM-SW — TPS65720/1 EVM Evaluation Software
I have download the above software and unzip the file after unzip its asking for .NET framework i have installed the framework also but still i am not able install the software…
Other Parts Discussed in Thread: TPS65720 Hi
I'm trying to run the TPS65720 GUI but it cannot see the USB bridge (USB Interface Adapter USB-I2C).
I can see when I plug the USB interface into the PC that it is installed as a HID compliant device.
My…
Part Number: TPS65721 Other Parts Discussed in Thread: TPS65720 Hi!
I faced with very strange error during continuous reading (more of 1 register data) from TPS65721.
My solution:
CPU: STM32F103CBTX
IDE: STM CubeIDE
Library: STM HAL library
I2C bus speed…
Other Parts Discussed in Thread: TPS65720 , TPS65070 , TPS80032 I'm looking for a Li-Ion/Multi chemistry battery charger/PMIC with provision to power load while charging the battery (I believe this is referred to as power path control ). The Battery connected…
Other Parts Discussed in Thread: CC3100 , TPS65720 , LP8340 , TPS63000 Hi,
I am working on PMIC for CC3100 mod and MCU.
The power source is Lilon battery. The tps65720 has a good performance but the WIFI module(CC3100 MOD) need about 1A current.
So can I…
Other Parts Discussed in Thread: TPS65720 Does the PMIC TPS65720 supply the full current from LDO(1.8V 200mA) and DCDC(3.3V 200mA) from the battery connected to it when there is no Ac input connected?
Hi Kelly,
Thanks for getting back to me. You were right, it was a typo, the part is the TPS65720 low power PMU:
www.ti.com/.../TPS65720
We are currently using this to power the DRV2604L and during startup, the device is not accessible from I2C. Currently…