Part Number: TPS659037 Other Parts Discussed in Thread: AM5728 , TPD12S015 Dear Sir,,
We are using AM5728 + TPS6590378 PIMC. However, it was changed to TPS6590379 PMIC due to difficult supply of TPS6590378. The power system was designed with reference to…
Part Number: TPS659037 Other Parts Discussed in Thread: TPS54335A In regards to support thread "TPS659037: Can I run the PMIC without OTP or modify the OTP"
Would it be possible to offer an ordering option for the PIMIC where OSC16M_CFG=1 without…
Part Number: TPS659037 Hello,
How to identify silicon revision ?:
On the part we see tps659037 OTP 97 1.3
Does it mean silicon revision 1.3, OTP 0x97 ?
Best Regards
Arie Paz
Part Number: TPS659037 Other Parts Discussed in Thread: AM5729
Hi All,
I would like to use TPS6590377ZWSR PMIC for my AM5729 processor application. In reference designs, there is DDR3 (1.5V supply) IC used but we want to use DDR3L (1.35V supply). Do I…
Part Number: TPS659037 Greetings. I'm investigating whether an external embedded controller can arbitrarily turn the rails on and off as well as set Vout and other VR parameters via I2C/SPI writes. That would effectively mean overriding OTP-programmed…
Part Number: TPS659037 Hi All, We are in the process of designing a new product using the Sitara Processor AM5728BABCXEA
Life cycle
1- Regarding the availability of the AM5728BABCXEA , I read the longevity policy TI has committed to.
This processor is still…
Part Number: TPS659037 Hi team,
My customer will use TPS6590379 and he considers to use 32kHz internal oscillator of the PMIC. Its register map states that OSC16M_CFG is type: "R" and Reset state: "X"
How can we enable 32kHz internal…
Part Number: TPS659037 We found Spike upto 13V on the Switch nodes of SMPSx_SW pins in TPS659037 IC.
Due to that spike, our PMIC chip is getting shorted between SMPSX_In and SMPS_SW.
Part Number: TPS659037 Other Parts Discussed in Thread: AM5728 , TMDSEVM572X Hi,
Please refer to the PMIC schematics on our custom board designed using AM5728, which has no dedicated power switch. See the related post for background information. The POWERGOOD…