Part Number: TPS65982 Hello, our company has been using your Texas Instruments TPS65982 for a long time, and we have some technical problems about this chip recently.
When we use this PD Controller chip as the PD chip, we borrow the above GPIO for operation…
Part Number: TPS65982 Hi Team,
When the customer was doing the test, he suddenly found that the retest rate was very high. Later, it was found that compared with the past code, he lost to add a Reset operation of this chip (TPS65982ABZBHR). Use this chip…
Part Number: TUSB1046EVM Hi guys.
I have TUSB1046EVM and TUSB564EVM. and i'd like to use as DP --> USB C --> DP signal converter.
so I connect both EVM Kit like below.
1. PC(DP out) --> DP Cable --> TUSB1046 and PC(USB) --> TUSB1…
Part Number: TPS65982 Other Parts Discussed in Thread: TUSB564RNQEVM , , TPS65987 , TPS65988 Hi, TI Support Team
The following inquiries have been received from customers.
The customer conducted a review with the TUSB564RNQEVM.
We developed the product according…
Part Number: TPS65982
Hi
I am using the TI TPS6598x Host Interface Tool to execute the DBfg function (clearing the Dead battery flag of the TPS65982 PD Controller).
I used a sniffer to capture the I2C communication between the Host Interface Tool and…
Hi Tommy,
The USB2.0 device's speed is 480 Mbps.
I am not sure why TPS65982 is picked over TSP65987, if it can fix this issue and can offer everything that the TPS65982 offers, we may use TSP65987 instead of TPS65982.
And how easy it to migrate to TSP65987…
Part Number: TPS65982 Hi,
I have a binary file which has been read off a TPS65982.
Is it possible to import the binary file into one of the programming tools in order to view the setup parameters for the chip? I do not have access to the original project…
Part Number: TPS65982 Other Parts Discussed in Thread: TPS65981 , TPS65987 We have a product consisting of 2 parts, both are powered by battery. When one of the batteries runs out of power, the other can supply power to it through USB-TYPE C, it will source…
Part Number: TPS65982 Other Parts Discussed in Thread: TPS65981 , TPS65988DJ , Hi,
Good Day.
I have a question about software TPS65981_2_6_7_8 Application Customization 6.1.4, does it fit TPS65982DJ? I have a broken laptop and the SPI flash of this TPS65982DJ…