The datasheet table 5 shows the possible addresses including 3 bits of ICB however there is only one ICB pin. How do I interpret this table? Do I ignore all but the 000 and 111 values for ICB?
Other Parts Discussed in Thread: TPS68470 Hi,
Customer is using TPS68470/GPIO5 as camera reset signal. The voltage level of this signal is 1.2V. I didn’t see any external pull-up on this signal, and assume it should be configured as a push-pull signal…
Part Number: TPS68470EVM-089 Other Parts Discussed in Thread: USB2ANY , , TPS68470 , IPG-UI Hi I'm using TPS68470EVM-089 + USB2ANY like below.
After power on TPS68470EVM-089 (check 3V3_SUS(3.3v), 3V3_VDD(3.3v) and LDO_IO(1.8v) in ACTIVE mode), connected…
Hi Stan,
The motor driver devices do not have an analog input.
The devices typically have a PWM input (either Phase/Enable or IN1/IN2) to control the H-Bridges outputs.
A quick search of products using "site:www.ti.com voice coil motor driver" identified…
Hello Frederik, The TPS657095 should work if the Buck converter is not needed. Please take a look at the TPS65217 and the TPS68470. The TPS65217 has 3 Buck converters and 4 LDO/LS with a WLED driver and host control through I2C.
Part Number: TPS68470GUI While trying to run the GUI for TPS68470EVM installed on Windows 10 it doesn't run and suddenly windows send a error message:
TPS68470 EVM has stopped working
A problem caused the program to stop working correctly.
Windows…
Other Parts Discussed in Thread: TPS65910 , TPS65912 , TPS65913 , TPS65917-Q1 , TPS65916 , TPS659039-Q1 , TPS659037 , TPS65217 , TPS80032 , TPS65090 , TPS65218 , TPS68470 , LP8720 , LP8725 , LP8733 , LP87565-Q1 , TPS65185 Many times people are looking for where the Linux…