Part Number: LM1117 Other Parts Discussed in Thread: LP5912 , TPS709 , TPS7B7701-Q1 , TPS7B4256-Q1 , TL1963A , TPS7A45 , TPS706 Hi team,
Does TI have some feature like this? the integrated back-to-back diode of LDO?
Like the below block. SGM2205.
Due to customer…
Part Number: TPS706
Hi application specialist.
Customer give us question,
Could you tell me alternative sockets of TPS70618DBVR if we have
Thank you for your kind help
Best
Yuki
Part Number: TPS706 Hi. If Vout is reinforced by another regulator, and Vin is allowed to fall below the Vout voltage, I expect that the reverse current blocking will cause the LDO to turn off.
Other posts have suggested that this isn't the case. Consider…
Part Number: TPS706 Other Parts Discussed in Thread: TPS7A05 Hi
1) Can the reverse current protection work even when the input is shorted suddenly? It looks that the internal comparator controls that function. I wonder if the comparator can work correctly…
Part Number: TPS706 Other Parts Discussed in Thread: TLV755 , TPS7A90 Hi team
1. Customer would like to use 100uF cap as output capacitor, because this cap will help when 1-msec instantaneous power failure happens.
Do you recommend to use 100uF cap…
Part Number: TPS706 I have a case where Vin is pulled from a 3.6V LiPo. To extend unit lifetime, we really want to run it right down to 3.0V. Iq is important.
Sometimes, the load needs to be driven with 3.3V. That will only happen when the charger is…
Part Number: TPS706 Hi,
My customer want to know how many the IGND when the output current is 1mA?
In datasheet, IGND is 1.3uA(typ) when output is 0, and 350uA when IOUT=150mA.
because they use battery to power the whole system, the IQ is very important…
Part Number: TPS706 Hi sir ,
I choose the TPS706 fixed output 3.6V for the MCU suppy.
when the input voltage higer than fix output voltage 3.6V , the TPS706 Iq is about 1.5uA .
But when the input voltage lower than fix output voltage 3.6, for example…
Hi Vishal,
We have not characterized the LP5907 at these levels of capacitors, so you may run into a stability issue.
We have plenty of customers using the TPS706 (and TPS709) in applications like this. I have looked at super capacitors on the output…
Part Number: TPS706 Can we have any data of the ground pin current at a few mA like Fig.10 in the datasheet for TPS70633 ?
It's a very important information due to battery application.
Thanks and Regards,
Metropolitan (Tokyo) Area FAE Kenji Nin…