Part Number: TPS767-Q1 I refer to the TPS 767-Q1 datasheet.
The P22 and p24 of this datasheet describe the thermal pad dimension information. The difference between these two pages is as follows.
(1) Dimensions of thermal pad are different. P22 :…
Part Number: TPS777 Other Parts Discussed in Thread: TPS775 , TPS767 Tool/software: Would you let me know about Min and Max value for RESET time-out delay?
Datasheet is described only Typ value: 200ms.
Best regards,
Satoshi
Part Number: ISOUSB211 Other Parts Discussed in Thread: TPS767
Dear TI,
Need some help in troubleshooting my own ISOUSB211 board used for computer-based audio playback.
I pretty much copied TI's EVM design with all external LDOs for both sides.…
Part Number: TPS777 Other Parts Discussed in Thread: TPS767 , From the TPS77725 datasheet:
"Like all low dropout regulators, the TPS777xx and TPS778xx require an output capacitor connected between OUT and GND to stabilize the internal control loop.…
Hi Kevin,
Unfortunately we do not have a higher current p2p device to offer for the LP2989. The LP2989 uses a unique pinout. The closest we have in that package is TPS767 and TPS777 .
Since we don't have a p2p perhaps we can suggest TLV767 or TPS7A47…
Hi Ashutosh,
Did the problem worsen if you just removed C3 and not C4?
The TPS767 datasheet recommends a minimum of 10uF even thought the stability plots show 4.7uF out Cout. Is there any chance you have other low ESR capacitors on the output…
Spanika,
We do not currently have a PSpice model for the UCC381. The TPS737, TPS767, or TPS768 may be of interest and I believe that they all have PSpice models available.
Hi Kishen,
The two ground pins are not directly connected within TPS767. 1GND is the ground reference for LDO1 and 2GND is the ground reference for LDO2. As such all pins and external components for LDO1 should be connected to 1GND. All of the pins…
Bret,
Thanks for taking a look. The last few days I've been debugging and found that the TPS767 was not producing the right voltage for 1.9V so I made some modifications and now it is outputing 1.9V and the debugger was able to pass the scan test…
Other Parts Discussed in Thread: TPS767 Hi, I am using ezdspf2812 kit from spectrum digital.promblem that i am facing is tps767 is getting heated up and the processor is looping back in init boot for free run but for single step the processor is running…