Part Number: TPS780 Tool/software: Good afternoon,
We are currently experiencing a strange behaviour on a TPS78001. The output of the chip is programmed to work at 3.2V, using a voltage divider in the output of R1=715k, R2=442k with a 10p cap in parallel…
Part Number: TPS780 Hi Sir,
My customer would like design TPS78001DDCT and would like to know the thermal information.
Would you please review table and provide feedback? Customer also request Thermal model PDML. Please advise.
Thermal resis…
Part Number: TPS780 Dear TI,
we are designing one product, after having discussion with TI we planning to use LDO in our device, but for initial stage we are looking for samples.
I gone through the website and for sample. after selecting the sample request…
Part Number: TPS780 Hello
would someone be able to clarify the drop out voltage of the TPS780330220 for me please?
I intend to use the device with an output voltage of 3.3v fixed and an input voltage of 3.6V and a load current of between 5-10mA.
I see…
Part Number: TPS780 Other Parts Discussed in Thread: TPS7A02 , TPS7A10 Hi,
Can two TPS780 be connected in parallel to double the output current?
Kind regards,
Part Number: TPS780 Hi colleague,
Our customer is using TPS78033022 to provide power to CC2652, TPS78033022 demand at least 1uF capacitor. If the customer wants to design the below circuit, whether it will influence TPS780 output?
Part Number: TPS780 Other Parts Discussed in Thread: TPS7A02 The TPS780 data sheet curves for ground pin current versus input voltage always stop at a minimum Vin well above Vout. What happens to quiescent current in the vicinity of Vin? Do you have any…
Part Number: TPS780 Hello,
I had a question on the TPS780230300DRV. I was looking through the datasheet and saw the recommendation about the input capacitance. Due to other functions on the same input line, I am looking to increase the capacitor to either…
Part Number: TPS780 Hi,
I have a question an application of this part. It is being used to switch 1.8 and 2.8 V to power some relatively low power components, < 30 mA. The input is a battery with voltage from 3-4.2 V. The switching is done with an…