Part Number: TPS784-Q1 Team,
Part number question I had a customer question about which part number to chose for the adjustable version of the device. I know it's the 01 version, but I was actually not able to find it in the datasheet.
Device protection…
Part Number: TPS784-Q1 Hi Expert,
Out customer is looking for LDO. The input voltage is 3.3V and output voltage is 3.1V. Output current is less than 150mA. The PG function is also needed. I only find TPS784-q1 with such dropout. Could you please help…
Part Number: TPS784-Q1 Team,
what is the Au plating thickness of TPS78401QWDRBRQ1?
I was not able to find it in the reliability and package data.
Best regards
Part Number: TPS784-Q1 Other Parts Discussed in Thread: TPS7A10 Hello Team,
I would like to use this part VSON 8 package.
From the datasheet, data for Vout versus Max output current is not available for my req.
Here is my req.
Vin= 1.8V +- 1%
Vout= 1…
Part Number: TPS784-Q1 Hi Team,
Is the only difference between the two part numbers the following?
TPS78401 B QWDRBRQ1: EN is pin 6
TPS78401QWDRBRQ1: EN is pin 7
Out of curiosity, what is the reasoning for the two different pinouts?
Thank you, Delane…
Part Number: TPS784-Q1 what is difference between using TPS78412 and TPS78401 FB tie to Vout? it looks like both can do 1.2V output and same schematics.
ito
Part Number: TPS784-Q1 Hi Team,
I found that TPS78412QDBVRQ1 is very suitable to our application, while I didn't found the Dropout Voltage vs Iout curve at Vout=1.2V. Do we have a test result curve on this fixed output version?
Thanks
BR
Frank
Part Number: TPS784-Q1
Hi,
I have a question about feedback resistor on TPS784-Q1.
I want to use the following four voltages: 3.0V, 2.8V, 1.8V, 1.2V
I calculated the resistor value through Equation 2, and I'm asking if there's any problem with using…
Part Number: TPS784-Q1 Other Parts Discussed in Thread: UA78L , TPS7B69 , TPS7B81 , TPS709 , TPS769 Hi Team,
There is a good new that we could DIN TI product!
Customer is looking for the replacement of SGM2203-5.0YK3G/TR
Please help suggest TI solution, T…