Part Number: TPS7A11 Other Parts Discussed in Thread: LP5910 , , TPS7A10 Hi team,
cusotmer would like to compare the PSRR curves of LP5910 and TPS7A11. Could you provide the PSRR curves that based on the following conditions? Vin: 2.0V Vout: 1.8V Iout: 300…
Part Number: TPS74801 Other Parts Discussed in Thread: TLV758P , TPS7A10 , TPS54525 Can we use LDO, TPS74801 for VIN = 1.7V and Vout = 1.5V application? Another words, to have Vout = 1.5V, can I have VIN = 1.7V only? In section 6.5 of its data sheet, it…
Part Number: TPS7A05 Other Parts Discussed in Thread: TPS7A10 , What's the maximum pull up resistance that can be put on the enable pin to minimize leakage current on this pin? Is this also the same for the TPS7A10?
Hi Yokota,
TLV700 will not work for your application due to the Absolute Maximum Rating for EN.
Please consider TPS7A10 to see if it fits your application requirements.
Very Respectfully,
Ryan
Part Number: TPS797 Other Parts Discussed in Thread: TPS782 , TPS7A10 , TPS7A05 Helllo,
I am looking for an LDO with:
very low quiescent current (sub microamp)
1.8V
50mA max
Small footprint
Low cost in volume
Only device I found is TPS797, are there…
Part Number: TPS780 Other Parts Discussed in Thread: TPS7A05 , TPS7A10 , TLV755P Hi Team, customer wants lowest Iq possible and requires 400mA peak current ( in short transients) is there an alternative to the TPS780 with similar Iq that can handle 400mA…
Hello
Just to be clear--The connection between bq24092 and Li-Ion battery should be direct with no additional components.
Between Li-Ion battery and CC2530 how to reduce the voltage from 4.2V to max of 3.9V. I would suggest a low Iq LDO, some to start…