Part Number: TPS7A15 Other Parts Discussed in Thread: TPS7A14 The datasheet specifies that different ouptut voltages are available in 25mV increments yet I see a much smaller set of parts available to order. Are there plans to add more? I am working on…
Part Number: TPS7A15
Dear TI Team,
A customer has raised a concern regarding the issue discussed in the E2E forum for TPS7A1510PDRVR.
According to the information posted, units bearing the following package marking were identified as belonging…
Part Number: TPS7A15 Other Parts Discussed in Thread: TPS7A14 , Re-opening thread here per customer request:
TPS7A15: TPS7A1510PDRVR 0.9V (not 1.0V) - Power management forum - Power management - TI E2E support forums
Part Number: TPS7A15 Other Parts Discussed in Thread: TPS7A14 Tool/software: Dear TI Support,
I have exactly the same issue as reported here: TPS7A15: TPS7A1510PDRVR . I see the problem with several devices.
VBIAS=5.2V
VIN=1.8V
VOUT=0.9V (should…
Part Number: TPS7A15 Tool/software: VCC_IN is 5V, and it outputs 0.9V with or without load at the end. It was tried to replace capacitors C286 and C287 with 10uF and C288 with 0.47uf. When the input voltage increased from 1.1 to 1.2V, the output was 0…
Part Number: TPS7A15 Tool/software: Hello, The datasheet specifies tSTR(typ) is 200us. But, how much us is the tSTR(min) and tSTR(max) respectively? Best regards, K.Hirano
Part Number: TPS7A15 Other Parts Discussed in Thread: TLV758P Tool/software: Comparing the recommended maximum output capacitors of the TPS7A15 and TLV758P, we found that the TPS7A15 recommends only 22µF, which is significantly lower than the 220µF recommended…
Part Number: DDS39RFS10 Other Parts Discussed in Thread: LMX2592 , , TPS7A94 , TPS7A15 , TPS7N53 , TPS62913
Tool/software:
Planning to use DDS39RFS10 in DDS only mode w/ DES (both DES2XL and DES2XH). Clocked with LMX2592 at ~7.1 GHz Fclk. Need some…
Hi Patrick,
What is generating the 3.3V rail? Also, what is the load requirements for the project or the expected load, is it only powering the DP83867IR?
This will help us provide a better suggestion for the LDO.
Perhaps looking into TPS7A14…