Part Number: TPS7A26 Other Parts Discussed in Thread: TPS7A25 Hi team,
Does TPS7A26 have an internal soft start to limit inrush current?
I found TPS7A26 product folder states the soft start function.
Also, it is discussed that TPS7A25 has the internal…
Part Number: TPS7A26 Other Parts Discussed in Thread: LP2989 Hi LDO folk,
I'm looking for SPX3819 replacement ;12VIN 3.3/5VOUT (adjustable type or fixed type). It looks the best fit is LP2989, but TPS7A26 is the newer device. Customer also can reduce…
Part Number: TPS7A26 Hi team,
My customer is using TPS7A2650DRVR, and it seems they have connected pin 2 (NC) to the output pin.
My expectation is that this will not impact the LDO operation in any way, since there is no internal connection, but I want…
Part Number: TPS7A26 Hi there,
it seems there is a large stock of TMS320F28377SZWTS (and TMS320F28377SZWTT). I am trying to order 5 pcs (or more), but I get always the message:
- Product(s) TMS320F28377SZWTT,TMS320F28377SZWTS cannot be supported by available…
Part Number: TPS7A26
Hi team,
My customer is using TPS7A26 in their project. The operation condition is shown as below.
Vin=5V (from DCDC)
Vout=3.3V
Cin=0.1+10uF
Cout=2.2uF
Load: two MCUs
The TPS7A26 has overshoot when start-up and the peak voltage…
Part Number: TPS7A26 customer having issue with TPS7A26 power/reset circuit performance.
datasheet indicates PG floats to the pull up voltage when Vout exceeds 93% of the targeted Vout voltage, and PG uses open drain to pull low when Vout drops below…
Part Number: TPS7A26 Hi,
Good Day. Customer wants to know the quiescent current of TPS7A26 when Vin=14V, Vout =5V, Iout=0.3mA.
As we check the datasheet, only Figure 10 and Figure 11 showing the quiescent current but Vout=1.24V and Iout=0A.
Can you help…
Part Number: TPS7A26 When i order the TPS7A2625DRVR, could not order it as below reason. But, all of other companies can order it. Please check what is the problem in our company.
Product(s) TPS7A2625DRVR cannot be supported from available inventory…
Part Number: TPS7A26 Hi team,
My customer is searching for a LDO. The requirement is
1. Vin=7.5V, Vout=3.6V, Ioutmax=500mA.
2. It needs to have EN pin and the Iq during disable status must be very low. when it is enabled, the iq during no load condition…
Part Number: TPS7A26 Hi LDO Team member,
We can’t find dissipation rating table of the TPS7A26.
Could you help to provide it?
For our appellation as below:
VIN = 12V
Vout = 3.3V
Iout = 0.05A
We need to confirm whether the above application meets…