Part Number: TPS7A30 Other Parts Discussed in Thread: TPS7A39 Hi team,
Customer get following spec request, could you help check if we get any suitable recommendation?
Vin: 5V, Vout: -2V ~ -0.1V(adj), Iout >=300mA;
Regards,
Will
Part Number: TPS7A30 For this device is the output voltage tolerance/accuracy independent of the dropout voltage?
So for instance, if I have an LDO with an input of 12.8 volts and output of 12V+/-2.5% (so 11.7 to 12.3V), and the droup out is 600mV.…
Part Number: TPS7A30 Other Parts Discussed in Thread: TPS7C023 Hi Team,
Do we have p2p replacement with SGM2209-ADJ SOT23-5? I only found TPS7A3001DGNR but it is not the same package. Thanks.
BRs,
Francis
Part Number: TPS7A30 Tool/software: Hi,
If this pin is shorted to 0V in order to force and hold the output to 0V, would that work ok in this device (Vin will remain -30V all throughout). For majority of the time, this soft-start pin will have a 1nF…
Part Number: TPS7A30 Tool/software: I listed some information below, along with a few questions, and was wondering if someone could help steer me in the right direction to help me understand and correct the issues I are seeing.
Also, who is the right…
Part Number: TPS7A30 Tool/software: Hi TIer
Do we have pin2pin alternative for XC62KN2502MR?
The customer would like to have undervoltage protection.
Thank you very much.
Part Number: TPS7A30 Team, Customer need following parameters of TPS7A3001DGNR for -12 vin to -5 Vout accuracy calculations
Designing operating temperature is -40 to 125 DegC.
temperature coefficient(V.TC value)
Value for error amplifier voltage…
Part Number: TPS7A30 1. what's the purpose of calculation Cout max? if Cout capacitor is bigger than this value, what's the impact?
2. where does the 140us comes from?
Part Number: TPS7A30 Other Parts Discussed in Thread: TPS65132 , Please help to provide the transient current value of this power supply.
Please review the background of below link.
The issue happens when connecting tps7a30 at output of tps65132,…