Part Number: TPS7A37 Hi
Let me ask you about connecting the NC terminal of TPS7A3701.
Should I connect the NC terminal and thermal Pad to a large-area ground plane?
Best regards,
Yokota
Part Number: TPS7A37 Hi, team,
I just need your help to confirm if below TPS7A3701 OCP waveform is a normal phenomenon or not. I cannot see detailed description about the OCP.
Thanks.
Johnny
Other Parts Discussed in Thread: TPS7A37 , CC3100 Dear Sirs,
I've found this TPS7A37 voltage regulator that seems good to power supply CC3x00 device.
From datasheet I've found:
"In the preregulated 1.85-V mode, the regulator providing the 1.85 V…
Hey Grady,
This is a large current range, do they expect to have it up to 1A? What do you mean by QOD?
For a 5V with 1A and reverse current protection I would recommend the TPS7A37 a low drop out regulator (see specs below).
TPS7A37
AEC Q100
NO …
Other Parts Discussed in Thread: TPS7A37 Hello ,
I found TPS7A37 as very tiny package device of 1A output LDO.
And 2.1V fixed voltage device is already launched, but adjustable version ans 2.5V fixed version are preview device.
Could you please kindy…
Hi Kevin,
Those results are what I would recommend given your requirements. I would go with the TPS7A37 as it is newer with better performance, if you can.
Thanks,
- Stephen
Part Number: TPS7A25 Other Parts Discussed in Thread: TPS7A37 Hi team,
We have an urgent support need below. Previous my customer is using the TPS7A37 to achieve the 3v to 1.5v (1mA) requirement. For the device's iQ is too large, they need to find P2P device…
Part Number: TLV757P Other Parts Discussed in Thread: TPS7A37 , TLV759P , TPS746
Hi team,
Is there a development plan to release TLV757P with 0.95Vout option?
If there is no plan, I will suggest TPS7A37 or TLV759P to customer for 1A power rail.
Regards…
Other Parts Discussed in Thread: TLV767 , TPS7A37 , TPS7A91 , TPS7A83A hi, Team.
could you tell me what device we might suggest based on below spec?
Vout:1.1V(fixed is suitable
Iout:1A over
Vin:5V(3.3v is also ok)
Hi Philip,
Thank you for your request.
I would take a look at our TPS7A37 which comes in a 2x2 package, the TPS7A91 that comes in a 2.5 x 2.5 package. Both of these devices have a max Vdo of 200mV.
Best Regards,
Wilson