Part Number: TPS7A4101 Hello, My customer has an question for current limit of TPS7A41. Is the current limit Brick-wall type or Foldback type?
Regards, Oba
Part Number: TPS7A4101 Hi Team,
In the datasheet of the TPS7A4101 it is mentioned that " the device can also withstand and maintain regulation during very high and fast voltage transients. These features translate to simpler and more cost-effective…
Part Number: TPS7A4101 Hi Team,
We are using TPS7A4101 device in a 24V power line (16V to 37V) which may face surge/EFT/ESD transients. We are planning to get 12V output from the LDO.
We have provided a surge protection device at the input with a clamping…
Part Number: TPS7A4101 Hello,
In my customer’s system, because there is a large input capacitance and there is no discharge load in this input circuit, about 3V remains for over 3 hours after power off.
I think it is not a problem, is it?
Regards…
Part Number: TPS7A4101 Hello, My customer has an question for TPS7A4101. They are considering to use it with AC24V input with half wave rectifier circuit. If the AC24V input is wrongly connected to OUT side like the below figure, could TPS7A4101 be damaged…
Part Number: TPS7A4101 Hello,
My customer has an question for TPS7A4101. The datasheet recommends to use 10uF capacitance for input.
In the customer’s system, there is a 100uF capacitance in front of the TPS7A4101 input capacitance(Cin) because they use…
Part Number: TPS7A4101 Hi,
Bellow is the operation condition.Because end customer need to test short circuit protect.
Our customer want to know whthere or not TPS7A4101 support short circuit protection?
If not could you give some advice.
Thanks
Vin…
Part Number: TPS7A4101 Other Parts Discussed in Thread: TINA-TI Hi Team,
I request the following data from customers.
· Bode plot of plant
· Bode diagram of FB line
Can these be obtained from WEBENCH?
Please tell me how to obtain it
Best…
Part Number: TPS7A4101 I would like to know the resistor values for a Vin of 28V and a Vout of 24V? I could not work the equation (Vref?????) I used Vin and it did not work out for values of R in the spec data sheet page #10.
Thanks,
Part Number: TPS7A4101 Dear Sirs or Madams,
If my understanding is correct, generally speaking the voltage on OUT pin of LDO should NOT exceed that on IN pin
in order to avoid the reverse current from OUT pin to IN pin.
But on our prototype board, the…