Hi Dalton,
Apologies for the delay.
1. For input voltage of 5V (USB), Vout = 3.7V and Iout max is 2.5A, TPS7A7300 will hit maximum Junction temperature supported by the device.
Below are the details.
LDO power dissipation (Pldo) = (Vin – Vout) * Iout =…
Part Number: TPS7A7300 Other Parts Discussed in Thread: TPS7A84A Hello,
Do you have measurment data or design estimation on noise variation of TPS7A7300?
Best regards,
Tetsuro
Part Number: TPS7A7300 Other Parts Discussed in Thread: TPS7A84A Hello,
Section 8.2.2.1 of the datasheet says grounding all of the ANY-OUT pin sets the output to 3.65V.
However, the note on Page.17 says to not use ANY-OUT pins for output voltages greater…
Part Number: TPS7A7300 Customer is using TPS7A7300 to power a cell modem. The VDD_CELL rail has 2 x 100uF 1210 package ceramic capacitors. These are big ceramics (GRM32ER61A107ME20L). What should the feed-forward capacitor value be? The data sheet states…
Part Number: TPS7A7300 Other Parts Discussed in Thread: LMK04808 , Hi team
My client configured the system with the following blocks.
LMK04808 does not work properly when testing -5 ° operation to chamber.
Normally, PLL2 should operate in cascade…
Part Number: TPS7A7300 Hello LDO Support Team,
Could I use two TPS7A7300 as parallel configuration for current sharing? I would like to double the output current of TPS7A7300.
Best regards,
Part Number: TPS7A7300 Other Parts Discussed in Thread: TPS7A84A , TPS7A89 LDO team,
One of our customers has built boards with the TPS7A7300 with output capacitance of about 1000uF. This is much higher than the max given in the datasheet of 200uF. What…
Part Number: TPS7A7300 Hi LDO Support Team,
Could I get the formula about soft start delay vs. Css? Do we have calculate sheet about it?
Best regards,
Alice
Other Parts Discussed in Thread: TPS7A7300 Hello, I am currently troubleshooting a design centered around the TPS7A7300. My reference datasheet is Rev.E (Dec 2015) By looking at the several figures, I notice that the pin 1 marker (circle) is situated near…
Part Number: TPS7A7300 We want to make a modification to a design that is using TPS7A7300. We want to output 5.3V instead of 5V for around 2A current (Vin of 5.7 or 5.8V).
What is the impact to do this?
Absolute max for "out" says Vin+0.3. If our Vin…