Part Number: TPS7A78 Hello @all
is it possible to use SDIN Pin of TPS7A7833 as a second DC-Voltage source? We want to switch a latched Relay with 12V or 6V for 20mseconds. (Current for 12V Relay:83mA, current for 6V Relay: 170mA)
Do you think this is…
Hi Y.Ottey,
As discussed, "The voltage from AC+ to GND will have 30V max and AC- to GND will have 30V max, per the datasheet and the clearance needs to be set accordingly".
When you mention input voltage, are you talking about the AC voltage…
Part Number: TPS7A78 Hello Team,
can I set the LDO_in voltage to 15V and use as intermediate supply and the 5V as a low voltage output? My goal is to use the device as a supply for gate drivers. So I need 15V for the FETs and 5V logic level voltage.
Thanks…
Part Number: TPS7A78 We need to be able to take power in from one of 3 AC input terminals, which we diode-or together. So the AC input would already be half-wave rectified. Can we feed this part with an already rectified source?
What is your expectat…
Part Number: TPS7A78 Other Parts Discussed in Thread: LM2903B Hello Team,
I downloaded Simplis software simulation (by Simetrix), in order to do simulation with the TPS7A78 models that are availaible on the product page.
My Simplis is working fine, but…
Part Number: TPS7A78 Other Parts Discussed in Thread: ISO7760 Hi,
I have a design using TPS7A7833PWPT in HB mode. Intermittently it powers up and LDO_OUT is 1.7V rather than 3.3V. I suspect it may have to do with me violating the Cldo_in/Cldo_out 10:1…
Part Number: TPS7A78 Hi Team, Our customer is Looking for AC to DC converter for power supply with the following information:
Input: 12V AC Output: 12V DC It's part of a basic transformer, rectifier, regulator power supply. This will need to support higher…
Part Number: TPS7A78 Dear team,
My customer was considering using TPS7A78 for their AC to DC power supply. But the requirement of output current is changed up to 300mA. But output current limitation of TAP7A78 is up to 120mA.
Is there any solution to…
Part Number: TPS7A78 Hi, Team,
I have 2 questions for TPS7A78.
1. Can TPS7A78 support the below DC input condition? Vin:~190Vdc Vout:6V? Iout:~0.1A
2. Is it possible to use TPS7A78 for 100Hz~900Hz AC power?
Best Regards,
Satoshi Yone