Part Number: TPS7B68-Q1 Dear experts,
Do we have small package version TPS7B6850-Q1? There are many NC pins for TPS7B6850-Q1. Customer don't want it.
Thanks
Part Number: TPS7B68-Q1 Hi,
The customer company uses TPS7B6850-Q1.
Line transient in the datasheet.
Vin : 6V to 40V(rising time 40us)
Vout : 5 V to 5.1 V (less than 100 mV)
The results measured on the customer PCB are as follows.
CH1 Vin : 13V to 40V…
Part Number: TPS7B68-Q1
In our schematic WD_EN, WD and WDO signals are connected to the microcontroller.
Whenever there is an issue in the microcontroller WD_EN signal will not be available from the microcontroller, also WD signal also will not be there…
Part Number: TPS7B68-Q1 In the datasheet:
" The correct watchdog service signal (WD) must stay high for at least 100 µs."
Then, what about this WD,must stay low for at least time?
Part Number: TPS7B68-Q1 Hello Team,
I have a question about TPS7B6850-Q1.
Is this OCP(Overcurrent protection) behavior Foldback? or Brickwall?
Thanks,
Yuta Kurimoto
Part Number: TPS7B68-Q1
Hi TI,
I want to pull up WDO_EN pin to disable the watchdog, can I connect the WDO_EN pin to 3.3V directly? Do I need to add a resistor to limit the current? How to understand below pulldown current in datasheet? Does it mean…
Part Number: LM73606-Q1 Other Parts Discussed in Thread: TPS7B68-Q1 , , LM73605 Hi, TI expert
7V DC-DC (LM73606-Q1) + 5V LDO (TPS7B68-Q1) We ask about the problem of output voltage when input power fluctuates.
The contents of the inquiry are as follows…
Part Number: TPS7B68-Q1 Hi team,
In Table. 3 of datasheet, it is written as 22uF + 0.1uF as recommended input capacitor.
Customer concerns if it's OK when input capacitor value gets bit larger due to capacitor variation by device.
Could you check…