Part Number: TPS7H1111-SP Other Parts Discussed in Thread: TPS7H1111EVM-CVAL Hi,
Is there any output impedance data for the TPS7H1111-SP?
I've simulated the output impedance at 0A and 1.5A using 2x100uF output caps and also simulated with a 1nF cap.…
Part Number: TPS7H1111-SP Hi,
I'm comparing the bode plots from the datasheet to the PSpice simulation included in the model.
I can't seem to match the plots well. What am I doing wrong?
Here is the circuit and some of the overlays.
Part Number: TPS7H1111-SP Other Parts Discussed in Thread: PSPICE-FOR-TI Hi experts
Are there unencrypted PSpice models available for this device?
Thanks,
Jim B
Part Number: TPS7H1111-SP Hi experts
Can someone comment on how to use OUTS for remote sensing when paralleling 2 devices to support higher load current needs?
Thanks,
Jim B
Part Number: TPS7H1111-SP Hello Team, I have been reading the document LDO Basics (slyy151a) from TI. The document refers to the capacitor DC voltage derating. In the image, the locked dipole seems to align with the applied electric field. While the active…
Other Parts Discussed in Thread: TPS7H1111-SP I am working a space system project that needs a linear regulator with the following characteristics:
Vout = 1.5 volts
Vin = 3.3V
Iout = 4.5A to 5A
Dropout voltage <= 200 mV with I Load = 750mA
Low noise…
Hi Tom,
We have noise data for this device up to 100kHz, which is the maximum of the range it was designed around.
There is a plot in this article which shows the noise performance of this device, as well as the TPS7H1111-SP (our Ultra-Low Noise, High…