Part Number: TPS84250 Other Parts Discussed in Thread: TPS84259
Tool/software:
Hello.
It contains 4x TPS84250 and 4x TPS84259.
The four TPS84250 outputs are set to +11.5V, because I connected a 133K 0.1% resistor between VOUT and VADJ, which is…
Part Number: TPS84250 Tool/software: Hello, I am using a DC/DC TPS84250 in my project with the "inhibit" function controlled via an FPGA.
Can you give me your opinion on the fact that when the inhibit is activated, my output voltage is not zero? It…
Part Number: TPS84250 Hi. I'm having a similar issue as explained on this ticket.
The only differences are:
Output voltage set to 12V
Frequency set to 800KHz
UVLO level set to 15V
All settings are based on Datasheet suggested values.
Part Number: TPS84250 Hi,
For our internal project we are using TPS84250RKGR step-down converter. Vin=28V, Vout=6V, Iout=1.21A, Fsw=500KHz. I have attached the schematics below. Kindly review the schematics and let me know the comments if any.
Part Number: TPS84250 Would the following scenario damage the TPS84250 ?
There is a very light load connected to the module and input voltage is disconnected and other circuitry drain the input capacitors faster than the output is dropping. Datasheet…
Part Number: TPS84250 Other Parts Discussed in Thread: TPS82084 Hi
I am using two new DC/DC modules for my design :
1.TPS84250 ~1.5A , 24V Vin to 5V
2.TPS82084 1.5A , 5V Vin to 3.3V Vout
I would like to reduce drametically the noise (EMC related…
Part Number: TPS84250 Hello,
Is the layer shown in Figure 41 in the TPS84250 datasheet supposed to be the layer directly beneath the top layer (Fig 40)? I.e. should Layer 2 be a PGND flood, with no AGND or PH present?
Thank you,
HSG
Part Number: TPS84250 Do we have the reverse breakdown voltage of the internal diode to PGND?
My customer needs this for his derating analysis.
Thanks for your help with this!
Richard Elmquist
Part Number: TPS84250 Hi,
We are using TI DC-DC regulator(TPS84250) in one of our design.For thermal simulation following information is required-
1. Material of the device
2. Density
3. Specific heat
4. Melting temperature
5. Resistivity
6. Thermal…
Part Number: TPS84250 Other Parts Discussed in Thread: LMZ35003 Hi,
Theses are two devices that seem identical: TPS84250 & LMZ35003
Both these devices have two ordering options each:
TPS84250RKGR
TPS84250RKGT
LMZ35003RKGR
LMZ35003RKGT
The…