Part Number: TPS84250 Do we have the reverse breakdown voltage of the internal diode to PGND?
My customer needs this for his derating analysis.
Thanks for your help with this!
Richard Elmquist
Part Number: TPS84250 Hi
First of all - I know that there's a new part number - LMZ35003RKGT
In the data sheet - in the 'thermal information' section there are some properties:
junction-to-ambient thermal resistance (θ JA)
junction…
Part Number: TPS84250 Hi Team, Customer asked about INH/UVLO pin. TPS84250 DataSheet shows INH/UNVL pin spec; ---- Parameter TestCondition Typ Max UNVL threshold No hys, Rise and Fall 2.5Vtyp VINH threshold No hys 1.25Vtyp 1.35Vmax ---- How shoul I understand…
Other Parts Discussed in Thread: TPS84250 , LMZ35003 Dear Team,
I have a customer trying to simulate the TPS84250.
While I couldn’t find a webbench link for it, the Spice model on the website is encrypted and cannot be used in TINA.
Do we have an…
Other Parts Discussed in Thread: TPS84250
This is how it is set up on both boards:
When we get a large current surge on another rail (not the +15 Volts), the input Vin droops enough that the power_good triggers and resets the TPS84250. The part does…
Other Parts Discussed in Thread: TPS54260 , TPS84250 Hello
Page 3 DS it is written:
(1) For output voltages < the minimum input voltage is 7V or (Vout + 3V), whichever is greater. For output voltages >12, the minimum input voltage is (1.33 x Vout). See…
Other Parts Discussed in Thread: TPS84250 Hi,
I have designed a small piggyback card using TPS84250 for generating the 12.5V@1A from 16-36V DC input. The board was assembled and tested and able to see the 12.5V coming. But when I connect the o/p to a load…
Other Parts Discussed in Thread: TPS84250 Hi guys,
Im designing a combo, which consists of 5V 2.5A DC-DC Buck with TPS84250, current/voltage sensor via I2C with SMSC PAC1710.
The design is almost finished, but I'd like to ask the experts to advice whether…
Hello Simple Switcher Team,
I have looked through the datasheets for both devices and they are nearly verbatum. Can someone enlighten me on the differences between these two devices?
Thank you for your help.
Ryan May
Other Parts Discussed in Thread: TPS84250 , TPS84259 Could anybody please supply me with the sugested foorprint and land pattern (with dimensions) for TPS84250 and TPS84259?
The datasheet curiously have nice drawings but no dimensions.
Many thanks in advance…