Part Number: TPS84621 Hi, I have been unable to find any in-depth material information for TPS84621RUQT. Can you tell me what the base material of the leads is?
Thanks.
Part Number: TPS84621 Hi,
Good Day.
Would like to know if the device can handle a 4A surge current at start-up from a device that it is feeding.
I have a device that has a 4A in rush current requirement and I would like to know if the TPS84621 can feed…
Part Number: TPS84621
Hi all
I have TPS84621 and 12VDC Input voltage.
Therefor in need to put an resistor network in front of INH/UVLO input right?
In the datasheet, there is only up to 10V (Table 9)
What resistors do I need to select? (I assume it will…
Part Number: TPS84621 Hi everyone,
I am using IC TPS84621RUQT in my application.
I need FIT rate of TPS84621RUQT for my module MTBF Calculation.It is not available in datasheet and that IC website page.
Kindly provide the FIT Rate of DC/DC Converter TPS84621RUQT…
Part Number: TPS84621 Hi,
I am using the TPS84621 Buck converter for my application to generate +3.3V from +12V. I need to use the UVLO feature. How to select the resistor divider network?
Details are not available in the Datasheet. Some fixed values…
Part Number: TPS84621 Dear Sir / Madam,
Please provide the ECCN Details of below mentioned parts:
1. TPS84621RUQT
2. TPS7A8500RGRT
3. TPS51200DRCTG4
Thanks and Regards,
Karthi P
Indus Teqsite (India) private Limited …
Part Number: TPS84621 Hey guys,
I am using TPS84621 in my circuit.
I am facing the problem in negative temperature with this Module.
Whenever it goes to low temperature, the module is turning off.
My load current is 1A (Imax).
Regards,
Santhana Krishna…
Part Number: TPS84621 Hey guys,
I am using TPS84621 in my circuit.
I am facing the problem in negative temperature with this Module.
Whenever it goes to low temperature, the module is turning off.
My load current is 1A (Imax).
Other Parts Discussed in Thread: TPS84621 Dear TI
Could you show me the HBM ESD Rating of TPS84621?
I need it for customer's inquiry.
Thank you & best Regards
K.Narisawa
Other Parts Discussed in Thread: TPS84621 , TPS84620 Hi All,
Can any one tell me reference voltage used in the feedback loop and its tolerance value for TPS84621 and TPS84620?
Thanks in advance.