Hi Thomas,
I would recommend you can change inductor from 220uH to 10uH and try again (Others can keep the same as the schematic you shared us first time). From my simulation, with 10uH, the output current is stable as 0.02A, as shown below.
L=10uH: …
Part Number: TPS923655DMTREVM Other Parts Discussed in Thread: TPS923655
Tool/software:
4188.TPS923655DMTREVM.pdf
0878.tps923655.pdf
I’m currently working on a backlight driver board using the TPS923655DMTR, I’ve configured the board to use boost and…
Part Number: TPS923655DMTREVM Other Parts Discussed in Thread: TPS922055DMTREVM Tool/software: Hi,
I have the following setup with TPS922055DMTREVM operating in flexible dimming mode:
ADIM/HD and PWM/EN frequencies are set @ 20 KHz and 240 Hz, respectively…
Part Number: TPS923655DMTREVM Other Parts Discussed in Thread: TPS923655 Tool/software: Using the EVM module to drive a string of LEDs. Vin = 24V. Vout = ~36V. Iout = 100mA - 500mA. PWM pin high. ADIM pin running a fixed 1Khz PWM sequence, set to give…
Part Number: TPS923655DMTREVM Other Parts Discussed in Thread: TPS922055DMTREVM , Tool/software: Dear Team,
My customer is going to evaluate the TPS923655DMTREVM and the TPS922055DMTREVM. They would like to refer the PCB layouts of those. Then, they want…
Part Number: TPS923655 Other Parts Discussed in Thread: TPS92641 Tool/software: This is a request from ongoing case CS2401818.
For our experiments it is necessary to
Control Frequency of the LED switching on and off(varying frequency from Khz - Mhz…
Hi Steven,
They use "PWM dimming mode" with ADIM/HD input pin = always H level by shorting between 1 and 2 of J7 on TPS923655DMTREVM and input 15us one shot pulse to EN/PWM pin.
Thank you and best regards, Kazuya Nakai.
Hi Gaston,
The prototype EVM is available in these links, for different IC packages:
TPS923655DMTREVM
TPS923655DRRREVM
TPS923653DYYREVM
The IC is currently in "PREVIEW" status on ti.com. Regarding the time that it is released to production, we can talk…