Part Number: TPS92520-Q1
Hello,
There are two buck in one TPS92520-Q1,if we connect the two output together, is there any risk?
On my view,when the MOS of buck1 is ON,and the MOS of buck2 is off, there may be current flow from MOS and power coil…
Part Number: TPS92520-Q1 I mean just use MCU to directly control the UDIM pin for ON/OFF.
but if unfortunately have a very noisy input such as a 12V with 3V 1KHz ripple, then some ripple on Boost (VIN for TPS92520) and on V5D. Is there any risk?
What…
Part Number: TPS92520-Q1
If we don't add output resistor in parallel with the Cout. When power off, will the output voltage fall slowly and the LED keep on for some time?
Or if 92520 has built in discharge circuit to discharge the CAP? If yes, where…
Part Number: TPS92520-Q1 Hello,
I would like to know if using the external PWM can only be done if the device is in standalone mode.
Does it mean that the PWM switches ON/OFF the device based on the by changing the UDIM input and act as enable signal…
Part Number: TPS92520-Q1 Hi team,
Our customer tested TPS92520-Q1 with VIN=57V, output capacitor=1uF. And in LED open circuit condition, they found VCSN waveform jumps between case1 and case3.
The problem is in case3, the time from fault occurs to read…
Part Number: TPS92520-Q1 I would appraciate to have a software application notes if there are, related to the Open/Short circuit detection for the three cases described in datasheet section : "7.3.15 Output Open Circuit Fault".
Part Number: TPS92520-Q1 Dear Sir/Ms.
My customer is asking how to measure Loop Gain. I have discussed with AE through Email before, and got AE's answer. But my client raised a new question as follows.
Q1: Customers want to know that GAIN / PHASE cannot…
Part Number: TPS92520-Q1
Hello Sir/Ms.
Do TI have TPS92520 Simplis model? My customer inquiry it. I just check with Customer RD. He want to use simulation tool to simulate gain margin and phase margin. If TI Don't have simplis model, Did TI have other…
Part Number: TPS92520-Q1 Can the TPS92520 (Gate Driver, Control logic...etc) operate normally when the Vin voltage drops below 6V > 4.3V? I'm sorry to trouble you. As I know the answer is Yes but customer want double confirm from TI.
Best Regards…
Part Number: TPS92520-Q1 Could you please kindly help to confirm how much current needed for TPS92520-Q1 V5A under normal work? Since we can only found V5A current under condition of stb and sleep mode, customer need to know the maximum current needed…