Part Number: TPS92633 Hello guys,
One of my customers is considering using the TPS92633 for their new product. Their requirements for the LED driver are as follows:
LED anode voltage: 30 V Number of LEDs in series: 8 or 9 LED current: 100 mA Number…
Part Number: TPS92633-Q1 Hello TI Team,
Could you please confirm whether a SPICE model is available for the TPS92633QPWPRQ1 ?
I would like to use the model for circuit simulation and design verification. If a SPICE model is available, please provide…
Part Number: TPS92633-Q1
Tool/software:
Hello,
I am using the TPS92633-Q1 in a 24V battery operation (16V - 32V).
I have connected 4 LEDs in series (for checking behaviour with 2 LEDs short)
My problem lies with open-LED behaviour.
I am…
Part Number: TPS92633 Is TPS92633MPWPR a pin-to-pin and functionally equivalent replacement for TPS92633QPWPRQ1?
Apart from AEC-Q100 qualification and automotive grade designation, are there any differences in silicon revision, electrical characteristics…
Part Number: TPS92633-Q1 When we conduct tests, each string of LEDs has two LEDs. If one LED is short-circuited, the other will dimly light up. This prevents the "ONE FAIL All FAIL" error from occurring.
Part Number: TPS92633-Q1
The schematics on the documentation are always represented with same numbers of LED connected to the all three outputs.
Could you please provide a schema with different output loads?
As example, which is the configuration…
Part Number: TPS92633-Q1 Other Parts Discussed in Thread: TPS92633 Tool/software: Hello,
I need Spice model for TPS92633 part. Need to simulate a design in Pspice for TI.
Part Number: TPS92633-Q1 Other Parts Discussed in Thread: TPS92623-Q1 , TPS92633Q1EVM Hi, AL team
TI korea team recommended TPS92633-Q1 to replace Competitor part number, TLD2311.
Can you confirm this is appropriate part? otherwise can you recommend…
Part Number: TPS92633-Q1 Tool/software: Dear responsible,
We are developing a CHMSL part for FORD with TPS92633QPWPRQ1. But we have problems with our thermal analysis. Can i ask for a meeting to get your support on the subject?
It’s a bit of a priority…