Hello,
I didn't understand, I thought there were two loads. You can use one board to drive for both of the loads.
Yes, TPS92691EVM-752 could work if the components are changed for higher current. The MOSFET, diode and inductor would be the main three…
Hello,
The TPS92691EVM-752 is set up for buck-boost (boost-to-battery) and will do 16V at 1A output from 9V-16V input. If you don't need PWM dimming you can just populate R22 and remove Q1, Q2, D2, R2, and R5. It's a good design.
Regards,
Cli…