Part Number: TPS929240-Q1 Tool/software: Hello:)
I was wondering if someone could help me to know the max power dissipated by the driver, I looked at datasheet but I didn't see this information.
Thanks in advance.
Regards
Part Number: TPS929240-Q1 Tool/software: Hi,
We are using TPS929240QDCPRQ1 LED driver . Can we know the max power it can support.
I calculated the power dissipation by the driver using the formula given in datasheet and we are getting power around 6W …
Part Number: TPS929240-Q1
Tool/software:
I have a requirement in which if any LED fails(open/short) or over temperature or under/over voltage then the device should automatically enter the FAIL_SAFE mode and turn of all leds.
As per TPS929240 datasheet…
Part Number: TPS929240-Q1 Tool/software: Hello, expert,
we need to change the default settings of TPS929240, need to operate EEP, is there any reference code implemented, please help to provide it or email it to me,
thank you.
Part Number: TPS929240-Q1 Tool/software: I am developing a prototype for CHMSL.
We will be using 37pcs Osram RGB LEDs (KRTBDWLM32.32) .
Each LED has a current of 10/50 mA.
Is it okay to run 8 LEDs (24 ports) on the TPS929240-Q1?
When the LEDs are operated…
Part Number: TPS929240-Q1 Tool/software: We are using TPS929240 to make a headlamp scheme;
When communication interruption is required, the chip output is turned off.
Since the chip watchdog is turned off by default, the watchdog needs to be turned on…
Part Number: TPS929240-Q1 Hello, experts.
DIAG Register (Offset = 7Bh) [Reset = X] In what scenario does the IRETRY parameter of this Register need to be modified, will it affect the accuracy of open circuit detection and short circuit detection? Please…
Part Number: TPS929240-Q1 Tool/software: Hello experts,
we plan to use TPS929240 in a new project. We plan to use the temperature sensor inside the chip to achieve thermal derating. We tested it on a PCB containing 8 929240, it is found that the temperature…