Part Number: TPSI3052-Q1 Hello, I would like to use TPSI3052QDWZRQ1 in a non Isolated Application, so in the system VSSP and VSSS would be the same. The reason I want to use this is becsue I want a 15V gate drive from a 5V supply. Is this acceptable …
Part Number: TPSI3052 Tool/software: Hi TI Support Team,
I am using the part TPSI3052 Gate Driver IC in my Current Design may I know what is the minimum and absolute Enable Current that is required for the gate driver IC (TPSI3052) when it is working…
Part Number: TPSI3052 Tool/software: Hello,
I have a question about the behavior of the VDDP supply in the TPSI3052. Would it be possible to switch the VDDP off for short periods, while keeping the Enable pin high and still get VDRV high on the secondary…
Part Number: TPSI3052 Other Parts Discussed in Thread: TIDA-050058 , TPSI3100 I have an application where I need to switch a boiler of max 3kw every 10 seconds. Hence I want to implement the following SSR circuit:
Can handle 230VAC
Max 13A continuous…
Part Number: TPSI3052-Q1 Other Parts Discussed in Thread: TIDA-050063 , TPSI31PXQ1EVM Tool/software: Hello TI team
I'm Zhuo Li, an electrical engineer from Sunwoda Mobility Technology Co., LTd(Tier1 battery system supplier).
Our department is very…
Part Number: TPSI3052-Q1 Other Parts Discussed in Thread: TPSI3052 Tool/software: Hi,
I'm using the TPSI3052-Q1 in my design in two instances:
1. as a driver to a high side SiC MOSFET in a similar application as the colleague complaining about the…
Part Number: TPSI3052-Q1 Other Parts Discussed in Thread: TPSI3052 , TPSI3100 Tool/software: Hi team,
My customer is using TPSI3052 in OCB product and met 89MHz EMI issue.
In datasheet, we see 89MHz is used for iso barriers communication.
…
Part Number: TPSI3052-Q1 Other Parts Discussed in Thread: TPSI3052 Tool/software: Hello,
We have the TPSI3052-Q1 designed into our product to drive a Mosfet in Three-wire mode. We have had a few instances where the the driver has failed with a short…