Part Number: TPSM33625 Tool/software: It would be very helpful to correct the datasheet accordingly, e.g. adding the information that the two SW pins should be connected together!
Kr
Part Number: TPSM33625 Tool/software: The TPSM33625 part receives a single +30VDC from our product and outputs four output voltages, of which the load currents of +4V and +3.3V are 0.6A and 0.4A, respectively. First, connect each load and apply the input…
Part Number: TPSM33625 Other Parts Discussed in Thread: TPSM33620-Q1 When can we expect TPSM33625FRDNR to be back in stock? It has been designed in to an important PCB and has gone out of stock just as we enter production. On a related question on TI…
Part Number: TPSM33625 Other Parts Discussed in Thread: TPSM84338 Hi All,
I have a question about the MSL for power module products.
The TPSM33625 and TPSM6361 products, released around 2022, will have an MSL level of 3.
The TPSM84338 and TPSM336xx…
Part Number: TPSM33625 Tool/software: Hi Experts,
We' like to ask assistance on the issue encountered by the customer with TPSM33625RDNR:
This schematic and board file applied on TPSM33625RDNR -the input voltage range [20v-26v] and the nominal voltage…
Part Number: TPSM33625 Tool/software: Hello Team,
We are using TPSM33625RDNR part for the 5V regulation. Input voltage will be 19V to 29.5V (29.5V Typ), total current on 5V is ~55mA.
We have observation that while we tuned off and turn on again…
Part Number: TPSM33625 Tool/software: Hello Team,
we have initiated one thread over etoe as follow:
TPSM33625: TPSM33625RDNR
In that we have below observation
Please find an attached requested input and output voltage and inrush current waveforms…
Other Parts Discussed in Thread: PSPICE-FOR-TI Tool/software:
TPSM33625 Transient PSpice Model
SNVMCA6.ZIP (655 KB) - PSpice Model
When I run the simulation using the example above, a window like the one below appear and the program close shortly…
Part Number: TPSM33625 Tool/software: Hello Team,
Good day!!
We would like to simulate a buck converter using the TPSM33625 IC. We obtained the PSpice model from the official Texas Instruments website. However, when attempting to import the model…
Part Number: TPSM33625 Tool/software: Hi,
In a new card that just arrived from assembly, a conversion circuit from 24V to 12V. The problem is that for some reason the circuit is in DROPOUT mode, meaning the output follows the input (minus DROPOUT voltage…