Thank you,
but my actual query is i have total system current is 7.135 A and i want to take 3 output form tpsm5d1806. The 3 output is 12v,3.3v and 5v .
Is this possible to get 3 different type of output in sigle 12A?
Part Number: TPSM5D1806 The datasheet of TPSM5D1806 lists four switching frequencies in Table 7-5. The MODE2 resistor sets the switching frequncy of the device, e.g 28.7 kOhm for 1.5 MHz, and 53.6 kOhm for 2 MHz.
Are only the discrete values of 0.5 MHz…
Other Parts Discussed in Thread: TPSM5D1806 , TPS541620 Hello,
Is there any equivalent power supply ic of TPSM5D1806?
if it is available please inform as soon as possible.
Thank you.
Part Number: TPSM5D1806 Hello team, I believe that there is an internal pull up resister in EN1 and EN2 pins. My customer would like to set EN pins to low when TPSM5D1806 power up. so they would like to use using pulll-sown resister. In this situation, they…
Part Number: TPSM5D1806 Hello
we have some queries regarding TPSM5d1806 device.
1. Does the spice model of TPSM5d1806 contain internal parasitic information? If not how to simulate the effect of internal parasitic?
2. The device supports two modes: dual…
Part Number: TPSM5D1806 Other Parts Discussed in Thread: TPS65279 Hi,
Section 7.3.3 of the datasheet for TPSM5D1806 talks about minimum recommended input voltages for various switching frequencies, but it doesn't say what happens if the recommended minimum…
Part Number: TPSM5D1806
Hello,
I have this design, in practice 3 parts failed after a few days of work, showing short circuit at the output.
I have further investigated one part after removing from the board and VOUT2 (pins 13-19) are showing zero ohm…
Part Number: TPSM5D1806 Hi,
Customer is looking for the value of the output voltage range of this device.
They are requesting if TI can provide the data/information regarding ripple voltage.
Thank you in advance.
Regards, Maynard