Part Number: TPSM5D1806 Other Parts Discussed in Thread: TPS541620 Hi team,
I want to output 1.2V and 5V from 12Vin with TPSM5D1806. The current is 4A each. The data sheet states that 2MHz is required to obtain 5V, but it must be 1.5MHz or less to obtain…
Part Number: TPSM5D1806 Hello team,
All ACM control devices including TPSM5D1806 have API(asynchronous pulse-injection) circuitry for improving transient performance?
TPSM5D1806 datasheet doesn't mention API in datasheet so I wanted to confirm if the…
Part Number: TPSM5D1806 Hi,
I'm trying to find a DC/DC power module with integrated inductor that able to sink AND source 20W. I need to place deux DC/DC in a push pull configuration.
I was thinking using the TPSM5D1806, is it a good solution ?
Th…
Part Number: TPSM5D1806 Hi TI,
I want to use TPSM5D1806 for my application. It can support input voltage 4.5V to 15V. The battery full voltage is 12.6 and above. but, when the engine is running condition the battery voltage is 13.7V to 14.7V.
1) What happens…
Part Number: TPSM5D1806 Please confirm the input capacitor connections in Figure 7-4 of the datasheet should connect PGND to pins 10,11 & 12 rather than pins 7,8,& 9
Part Number: TPSM5D1806 Hello
Could you review the attached design file?
TPSM5D1806 is used as 2 independent outputs.
Condition :
12V TO 5V, 3.3V (External EN Control)
12V TO 3.3V, 1.2V (EN High Fixed)
TPSM5D1806 SCH.pdf
Best Regards
Part Number: ADC12DJ5200RF Other Parts Discussed in Thread: DAC39RF10 , , TPSM82913 , TPSM5D1806 Hi,
Could you recommend which power supply can be shared in this multiple ADC+DAC application?
Customer would like to 5 combination of ADC12DJ5200RF and DAC39RF10…