Part Number: TPSM63603
Hi team,
our customer wants to use the TPSM63603V3, so the version with fixed 3.3V output.
Currently, we only see the 1% tolerance of the VREF, but there's no indication of the tolerance of the resistor divider.
Do we have this…
Part Number: TPSM63603 Hi team,
Is it okay to connect LDOIN to VOUT at 12Vout? I believe that there are cases where the transient response and resistance accuracy exceed 12.5V.
Best Regards,
Part Number: TPSM63603 Hi team,
In customer application, sync will firstly apply to tpsm63603 and then Vin will apply. With Rent=560kohm,Renb=100kohm, TPSM63603 can't power on. But with Rent=Renb=100kohm, TPSM63603 can power-on normally. Could you…
Part Number: TPSM63603 Other Parts Discussed in Thread: PMP , TPSM63606 , LM61460 Hi team,
Here is several application details of TPSM63603 want to confirm with you.
Q1: if we want to achieve a adjsutable output based on TPSM63603, if it's accepatable we…
Part Number: TPSM63603 Hello team,
Can I think TPSM63603 is RoHS compliant device?
If above is yes, when will it be updated in below link?
https://www.ti.com/quality-reliability-packaging-download/report?opn=TPSM63603RDHR
Best regards,
Part Number: TPSM63603
According to the datasheet, 6.5 Electrical Characteristics it states:
VIN Input operating voltage range - Needed to start up (over IOUT range) - 3.95V
Does it meen that it is not possible to start up this device from a standard…
Part Number: TPSM63603 Team,
It seems that the Ultralibrarian CAD file (detailed view) for RDH footprint (see below link) does not include all dimensions from our drawing provided at page 28/29 of the datasheet SLVSFS5:
https://www.ti.com/product/TPSM63603…