Part Number: TPSM63603EVM Tool/software: Hello,
Are the schematic and/or layout native files available for the TPSM63603EVM ?
This has the:
TPSM63603RDHR, with VinMax = 36V, Vout from 1-16V, at up to 3-A, step-down power module on it.
Thank you in advance…
Part Number: TPSM63603EVM Other Parts Discussed in Thread: TPSM63606 Tool/software: Dear Sir/Madam,
we have design and develop TPSM63606 circuit which provide +15V to +5V output but it is not working giving expected output +6.3V .
it is showing output…
Part Number: TPSM63602 Other Parts Discussed in Thread: TPSM63603EVM , Tool/software: Hi team,
In order to evaluate TPSM63602, should I use TPSM63603EVM?
If so, do I need to replace the device on the EVM by TPSM63602?
Best regards,
Kazuki Itoh
David-san, Thank you for your response. Just to confirm. The customer is using TPSM5D1806EVM and TPSM63603EVM. Then checked the input Ripple with EVM, so I think that the layout is not so bad. I will ask the customer to add large Input capacitance such as TPSM63610EVM…
Hi BX27,
1. Yes you can use the TPSM63603EVM to test Sync, just make sure to remove J5 before.
2. In an application context you are correct, and yes, this was even done on the EVM. (see below)
For the EN/SYNC pin you talked about earlier, it may not have…
Part Number: TPSM63602 Other Parts Discussed in Thread: TPSM63603EVM For the chip TPSM63602,
1. the data sheet give a recommended layout, but that does not connect the VOUT pins to the FB and VLDOIN pins,
I want to know what is the recommended approach…