Part Number: TPSM63604 Other Parts Discussed in Thread: TPSM64404 , TLVM13640 Hi team,
Our customer is considering adopting the TPSM63604. The intended operating conditions are as follows: an input voltage of 20–30 V (typical 24 V), and two output…
Part Number: TPSM63604 Tool/software: We have a TPSM63604 as the input stage SMPS on our design. There is TVS protection, CLC filter, and reverse protection stage with soft start on the input. We had an instance where we plugged two of our modules into…
Part Number: TPSM63604 Other Parts Discussed in Thread: TPS61288 Tool/software: We are having issues getting the power supply to come up to +12V. Here is the schematic:
The supply only comes up to 4.5 volts - we notice a note in the datasheet which…
Part Number: TPSM63604 Tool/software: Hello,
I am trying to find the calculator sheet for this power module, but the page seems to miss the actual calculator: https://www.ti.com/tool/TPSM6360XDESIGN-CALC
Br. Thomas
Part Number: TPSM63604 Tool/software: Hi,
In the calculator spreadsheet, a junction temperature is calculated (estimated) of 64 degrees.
Under what circumstance is that, in the spreadsheet the demo board is shown? I have the demo board and with…
Part Number: TPSM63604 Tool/software: Hi experts,
My customer want to know the maximum supported output capacitance of TPSM63604. The datasheet only provide minimum output cap, no data for maximum. They want to use as large as possible output cap to…
Part Number: TPSM63604 Other Parts Discussed in Thread: TLVM13640 ,
Tool/software:
Hello,
We are designing 2 buck regulators with TLVM13640 and TPSM63604. We are using TPSM63604 for 12V output and TLVM13640 for 5.3V output. Can someone check below…
Part Number: TPSM63604 Other Parts Discussed in Thread: TPSM33625 , , TPSM63606 Hello Technical Team ,
We have requirement to design Multiple Output Power Supply as per attachment. I have to design it Compact and as per Automotive /MIL Grade. I have…
Part Number: TPSM63604 Hi,
I was wondering how the adjustable SW Slew rate function work. As far as I am concerned, one way to slow down the slew rate is increased the gate resistor, Is this function works also in this way?
If yes, compared to the…
Part Number: TPSM63602 Other Parts Discussed in Thread: TPSM63603 , TPSM63604 , TPSM63606
for devices TPSM63602, TPSM63603, TPSM63604, TPSM63606
I am not able to find the following information in the datasheet/application notess
whether
1. all…