Part Number: TPSM63606 Tool/software: It was manufactured from +15V to -15V using the tpsm63606 IC.
However, it generates heat even when not loaded,
and when operated up to 2.5A with an electronic load, the heat goes out of control.
I understand…
Part Number: TPSM63606 Tool/software: Hi,
We are in urgent need of these chips. Preferably the S (spread spectrum) variant. Any option to get them? We can not find them at our regular distributors.
Thanks,
Luca
Part Number: TPSM63606 Tool/software: Hi ,
I have designed a DC-DC Reg circuit Using the TPSM63606 IC.
Input voltage is 15VDC and the O/P voltage is 12V@6A Rating. When i am doing the testing i am getting the O/P voltage as same as the I/P voltage…
Part Number: TPSM63606 Tool/software: Hi,
I would like to use TPSM63606SRDLR in my design, but I can't find it available anywhere. When will it be back in stock?
Thanks,
-Jorge
Part Number: TPSM63606 Tool/software: Hello,
I'm looking forward to receiving your best quotation for 50pcs of TPSM63606 item.
I need you support, I'm in italy and I'm a distributor.
Many thanks and best regards
Part Number: TPSM63606 Other Parts Discussed in Thread: TPSM63608 Hi experts:
Can TPSM63606 support output 12V@6A with 15V input?
I am searching for a solution to regulate 15V input to the output 12V@6A.
Can TPSM63606 work for this?
Thanks,
…
Part Number: TPSM63606 Tool/software: Hi. We've been using some TPSM63606 parts for reducing input voltage from typically 28V to output either 12V, 5V or 3V3 rails. However we have one application where we would actually need to use it with a 5V input…
Part Number: TLVM13660 Other Parts Discussed in Thread: TPSM63606 , Tool/software: Hi, I will change device from TPSM63606 to TLVM13660 because TLVM is much lower than TPSM. My use case is Vin is 24V and Vout is 5V (Iout 3A - 4A). So TLVM can work correctly…
Part Number: TPSM63606 Tool/software: Hi ,
I want to use the P/N:TPSM63606 for one of my 12V/3A O/P Requirement. I want to know for the 12V O/P what is the minimum I/P Voltage is required. I have the Input DC source of 15V(if required i can bring upto…