Part Number: TPSM63606 Other Parts Discussed in Thread: TPSM53604 Hi Experts,
Good day.
If I want to design a positive input to provide negative output (-15V) using TPSM63606, is it possible?
I could see that PGND and AGND from its typical example of…
Part Number: TPSM63606 Other Parts Discussed in Thread: LM25145 , LM25148 , LM25149 , LM61495 We need 3.3V with 8..10A out of 10..30V with high efficiency, very limited space, low EMI and synchronised switch frequency above 2MHz. We prefer fully integrated…
Part Number: TPSM63606EVM Other Parts Discussed in Thread: TPSM63606 Tool/software: Hi TIer
Customer want to use TPSM63606 in 4 series lithium battery system.
So input voltage max is 4 * 4.2V
To allow the battery to discharge more fully, the customer…
Hi Jonathan,
Here are a couple of application notes which explain how to configure a device for the IBB topology.
General IBB: https://www.ti.com/lit/an/snva856b/snva856b.pdf
IBB with a Module: https://www.ti.com/lit/an/snva897/snva897.pdf
When using a…
Part Number: TPSM63604 Other Parts Discussed in Thread: TPSM33625 , , TPSM63606 Hello Technical Team ,
We have requirement to design Multiple Output Power Supply as per attachment. I have to design it Compact and as per Automotive /MIL Grade. I have selected…
Part Number: TPSM64406 Other Parts Discussed in Thread: TPSM63606 , Section 6.4 (Thermal Information) of the December 2023 datasheet only lists two metrics for the package/device thermal information.
Datasheets for other devices (e.g. TPSM63606) in this…
Hello Sandeep,
For the switching Reg, please consider the LM61460, we also have modules with integrated inductor also, please consider the TPSM63606.
Hope this helps,
David.
Part Number: TPSM63606E Dear Sir/.Madum,
We Are Using TPSM63606 IC for Generating 5 V ,10 V . But The Calculation For Frequency Is Confusion. As Per The Datasheet Give The Value For 5 V But Not For 10 V ,
Kindly Give The Calculation For Frequency Resistor…
I think LM25085 isn't a good choice because it require external MOSFET. I found another BUCK IC TPSM63606 but it's BOM cost is very high. The 3rd option i found TPS56837 but it requires 5V for PG and i don't have this supply in the system Any…