Part Number: TPSM6360XDESIGN-CALC I am looking to calculate the efficiency of several TPSM6360X modules under various conditions, I planned to use the TPSM design tool on the webpage which looks like it would support what I am looking to do, but I don't…
Hi Tony.
The recommended switching frequency for a 12V output is quite high with this module (to maintain a reasonable 30-50% the inductor ripple current at Vin = 24V, 36V, etc.).
However, if the Vin-max of your application is low (e.g. less than 18V…
HI Olivier,
The intention here is to set the ripple current at 30-40% of the 6A rated load (for optimal copper/core loss balance in the inductor) and also to match the internal slope compensation ramp. This can be checked with the TPSM63606 quickstart…