Part Number: TPSM64406 Hi,
I am developing a power supply with a 12 V to 35 V input and a 5 V / 12 A output, using two linked TPSM64406 devices in a four-phase configuration.
In the attached TPSM64406 datasheet, page 19, Figure 7-4, High-Efficiency…
Part Number: TPSM64406 Other Parts Discussed in Thread: TLVM14406 Hi team,
The TPSM64406 datasheet states that the device can be used to generate a negative output voltage. In this context, is it possible to configure only one of the two outputs as…
Part Number: TPSM64406 Tool/software: Hi Team,
We are using the TPSM64406RCHR in our design, configured for a 12 V to 4.2 V step-down conversion. The 4.2 V output serves as the main power supply for our SOM module.
During certain test cases, the system…
Part Number: TPSM64406 Hi,
We consider to use TPMS64406 for the dual channels output design, and one channel output voltage is 15V and the other channel output voltage is -15V, and please advise if this device is available for this request, thanks.
Part Number: TPSM6440X-DESIGN-CALC Other Parts Discussed in Thread: TPSM64406 I am trying to simulate the model of TPSM64406 in LTSpice,
issue in decrypting the library as your pspicemodel is encrypted.
Kindly provide unencrypted model;
Part Number: TPSM64406 Hissing sound observed from the module & Module was heating more. Because of over heating complete board was heating. But Module was giving proper Dual output voltages.
Now we are using the few projects, so can you please let…
Part Number: TPSM64406 Hissing sound observed from the module & Module was heating more. Because of over heating the module complete board was heating. But Module was giving proper Dual output voltages.
Now we are using this in few projects, so can…
Part Number: TPSM64406 Hello team, I have 2 questions to determine FB resisters. Would you please advise?
Question 1: About determining the FB resistor I have a question regarding the recommended method for determining the feedback resistors. The datasheet…
Part Number: TPSM64406 Tool/software: Hello team, My customer has some questions. Would you please advise? 1. The customer would like to use TPSM64406 as the following condition. Is it possible to use the following condition? Vin = 14V Vout = 2.5V Iout…
Part Number: TPSM64406 Tool/software: Hello, I need clarifications on the length of some of the pads given. See image for missing dimensions needed. And if it's possible, please expedite.