Part Number: TPSM82810 Tool/software: Hi Teams,
Regarding the heat dissipation method of TPSM82810SILR, a power chip with a large capacitor on top, can it be attached to the metal casing for heat dissipation? thank you.
Do you have any good suggestions…
Part Number: TPSM82810 Other Parts Discussed in Thread: TPSM82816 Tool/software: Hi Team,
Customer is having below query on webench simulation and default values selected, can you please help on the same.
For setting up the mode, why did Webench…
Part Number: TPSM82810 Tool/software: Is there any index marking for the top side (where the inductor is mounted) for TPSM82810? I've looked at pictures of the regulator online, and also checked the 3D model in detailed version, but it is not clear to…
Part Number: TPSM82810 Hi team,
In D/S, ramp time (tRAMP) is 100 to 200 [us].
However, it seems to be more long time in start-up timing figure. Can I use this IC as tRAMP less than 200us?
Best regards,
Goto
Part Number: TPSM82810 Tool/software: Hi team,
We found the copper keep-out area requirement on the example board layout, and want to make sure it is required on the device layer only, or on all other layers. Thanks!
Regards, Sam Ting
Part Number: TPSM82810 Hello,
My customer is designing for the first application of TPS82810.
Could you please review the customer circuit and PCB design below?
TPSM82810 SCH_PCB.pptx
Thank you.
JH
Part Number: TPSM82810 Other Parts Discussed in Thread: TPSM82816 Dear Specialists,
My customer wants to simulate TPS82810 with Webench.
The circuit was opened using the initial settings in WEBENCH.
When they try to change select ambient temperature…
Part Number: TPSM82810 Hi,
Q1: Could you give me the temperature profile material for reflow?
Q2: Also, is there anything I should be aware of when implementing?
Q3: Finally, could you tell me the reason why Via is placed under the pin, like P30…