Part Number: LMZ10503EXT Other Parts Discussed in Thread: TPSM82813 Hi,
I use the WEBENCH to simulate the bode plot for LMZ10503EXT.
This condition of the design is as below.
Vin (min/max) = 3.1/3.5
Vout = 1.05
Iout max = 1.5
Temp = 30C
The bode plot…
Part Number: TPSM82821A Other Parts Discussed in Thread: TPSM82813 The data sheet for the TI regulator TPSM82821A states the following.
Is this the capacitor placed only next to C306 (22μF)?
An FPGA whose internal power supply voltage is 1.0V generated…
Hi Eugene,
There is no plan to stop the TPS82085. There are supply constraints at the moment. TPSM82823 and TPSM82813 are the recommended alternatives.
Best regards,
Varun
Hi Moheddin,
Thanks for your help.
If the customer deems necessary, may a thermal pad be applied to the top of the module when using the power module below?
- TPSM82823
- TPSM82864A
- TPSM82810
- TPSM82813
Thanks,
JH
Other Parts Discussed in Thread: TPSM82822 , TPSM82813 , TPSM82810 , TPS62442-Q1 Hi TI Team,
I am looking for an alternate/similar (EN5329QI, EN6347QI Non-Isolated PoL Module) DC DC Converter with below features.
1. Regulator 1 features: Non-Isolated PoL Module…
Part Number: TPSM82810 Other Parts Discussed in Thread: TPSM82813 , Hi,
What is the difference betweenTPSM82810 and TPSM82813?
They have same data sheet and I couldn't find no difference on it except output current..
Do they have same specs?( For example…
Part Number: TPSM82864A Other Parts Discussed in Thread: TPSM82813 , Hi team,
Are there some difference of Electrical characteristics between TPSM82864AA0 and TPSM82864AAH?
Best regards,
teritama
Part Number: PTH04070W Other Parts Discussed in Thread: TPS82085 , TPSM82813 , TPSM82823 Hi Team,
The customer is asking your opinion about the design below. This use PTH04070 to convert 5 V to 1 V. Please see the schematic below and see if it's okay or not…
Part Number: TPSM63606 Other Parts Discussed in Thread: TPSM82821 , LMR51420 , LMZ31506 , LMZ31704 , LMZ31503 , TPSM82810 , TPSM82813 Hi Team
My customer is considering using TPSM63606 for Enpirion replacement, but has concerns about the output voltage range…
Hi Dan,
Unfortunately, we can not support the request currently due to shortage and please check on distributor like arrow or digikey.
If they do not have any supply you could check these 2 devices which could fit:
TPSM82810 data sheet, product information…