Part Number: TPSM82902 Other Parts Discussed in Thread: TPSM82901 , TPSM82903 , Hello,
Is there any differerence in efficiency or EMI performance between the TPSM82901, TPSM82902, TPSM82903 when outputing less than 1A? The switch characteristics and…
Part Number: TPSM82902 The TPSM8290x devices are not available and no form, fit and function alternates seem to be offered. I have 2 questions: 1. When does TI plan on having these devices back in inventory? 2. What solutions have other designers facing…
Part Number: TPSM82902 Tool/software: Hi Team,
As the details below - it supports discrete and fixed VOUT voltage as per the R2 selection.
Does this part supports dynamic and continuous VOUT vs VSET ? Can I bias the VSET node with a variable voltage…
Part Number: TPSM82902 Tool/software: Hi Team,
I am using TPSM82902SISR IC with Vin - 12V and Vout - 1.8V. I have attached the schematics snap for reference.
/resized-image/__size/320x240/__key/communityserver-discussions-components-files/196/pastedimage1740405263204v1…
Part Number: TPSM82902 Dear Team,
I have attached TPSM82902SISR schematic for review. Could you please check and provide your feedback. The output voltage selected is 2.5V
Regards, Irfan
Part Number: TPSM82902 Hi Team,
We are using the TPSM82902SISR as a 12 V to 2.5 V, 2 A regulator in our design. However, instead of providing the expected 2.5 V output, it is generating 3.3 V. We have checked the output rail for shorts, and no shorts…
Part Number: TPSM82902 Tool/software: Hello,
Can TPSM82902SISR be used as a power supply for termination resistors VTT (OCT) of an FPGA in DDR2 application?
Best regards,
NM
Part Number: TPSM82902 Dear Team,
Since i was facing a back drive issue in TPSM82902SISR so could you please recommend any Regulator which does not require output inductor and also should not back drive voltage from output to input.
Req: Input voltage…
Part Number: TPSM82902 Tool/software: Dear Team,
We are using the TPSM82902SISR in our design. The input to the module is 12 V , and the output is regulated to 5 V . This 5 V rail is also routed to an HDMI port.
We are facing an issue with backdrive…
Part Number: TPSM82902 Tool/software: I am using some of the TI regulator parts in my deign, and attached PDF format for the review. Please provide your comments for the same. Power Section - TI parts.pdf