Part Number: TPSM8A28 Hi team,
My customer found TPSM8A28 efficiency gap from the datasheet.
He would like to check VIN=12V, VOUT=5V, IOUT=4A, 600kHz FCCM frequency of TPSM8A28.
In the datasheet Figure8-9, it looks like ~93%. But the Webench shows that…
Part Number: TPSM8A28 Hi team,
My customer concerns about the reflow of TPSM8A28. My customer is likely to place these modules on the first reflow side. So they concerns about the risk which the modules drop off from PCB during the second reflow like discussed…
Hello,
TPSM8A28, TPSM8A29 are the closest device that can do 15A with only 1 input, it is COT (DCAP3), module with 12VIN nominal and is analog only. is has remote sense.
Thanks
Tahar
Part Number: TPSM8A29 Other Parts Discussed in Thread: TPSM8A28 Hi team,
Is the efficiency curve on the TPSM8A28/9 datasheet applicable for both TPSM8A28 and TPSM8A29?
Or, does it have any difference?
The current range looks <15A which is only supported…