Hi Itoh-san,
The datasheet has been revised and is waiting for finally approval to release to ti.com this week or next week. Please double check the draft as attached here. Thanks for pointing out all errors.
Tri-ccfffce1-8790-4cc5-928d-16ba40cb89e3.p…
Part Number: TPSM8D6C24 Hello,
My customer has a design where the top resistor of ADRSEL_A is 1.1kOhm and the bottom is 10kOhm. Based on the datasheet, this seems like it corresponds to address 0x24h (36d). But the device responds to 0x14h (20d) instead…
Part Number: TPSM8D6C24 Hello,
My customer is concerned about how to design core power.
1. What is the difference in efficiency between Case-A1 and Case-A2?
If the conditions are the same, which case has the advantage in terms of efficiency, and is there…
Part Number: TPSM8D6C24
Hi
The design is DC/DC from input 5.5V and output 0.95V , Current 46A. A and B connected tougher
I need help in Design review and need layout support
Please attach file my design and please review and comments
As I understand…
Part Number: TPSM8D6C24 Can the TPSM8D6C24 be used as the core power supply for Agilex FPGAs?
I guess that the PMBus master function of Agilex cannot be controlled unless address 21h (VOUT_COMMAND) and address 8Bh (READ_VOUT) completely match at 1LSB voltage…
Part Number: TPSM8D6C24 Hi
I need to get 0.95V in the Vout, I try to understand the calculation
according to table 7-12:
Resistor divider code = 2
Code = (0.95-0.9)/0.01 = 5
So in this case, I need 2 resistors from Vsel Pull up to BP1V5 and Pull down…
Part Number: TPSM8D6C24 Other Parts Discussed in Thread: TPSM8D6B24 , Hi all,
Is there safe operating area curve data available for this device? If so, would you be able to provide it or is there more contextual information needed for that data?
Regards…
Part Number: TPSM8D6C24 Hello,
My customer inquires for additional information required for system design.
Could you please give them the height information shown in red below?
Thank you.
JH
Part Number: TPSM8D6C24 Hi,
We use TPSM8D6C24 as PMIC and place remote sesing on loading side, the resistor is 49.9R based on TPSM8D6C24EVM reference design.
Is it possible to increase or decrease the remote sensing function effect by modify the resistor…
Part Number: TPSM8D6C24 Hello E2E,
I’m using TPSM8D6C24 in a dual-phase operation to power the core rail for an FPGA/processor. This controller has “SVID” (SmartVID) to throttle the voltage and increase efficiencies. It requires a standard PMBUS interface…