Part Number: TRF7962A Other Parts Discussed in Thread: TRF7964A , TRF7970A Dear Specialists,
My customer is considering TRF7962A and has a question.
I would be grateful if you could advise.
---
Regarding TRF7962ARHBT datasheet,
There are input VIL, VIH…
Part Number: TRF7962A Other Parts Discussed in Thread: TRF7964A , TRF7970A Hi,
I am working on a project to achieve ISO15693 label read and write data based on trf7962A chip. I have a hardware board that matches the example code of TRF7960EVM (sloc251…
Hi, There was no feedback since a while, so I assume this tread is resolved and can be closed. You can still reply to this thread after it is closed, or you can create a new thread. Best Regards, Andreas.
Hi, I haven’t heard back from you for a while, so I will close this tread. If you wish to continue the discussion, please post a reply with an update below (or create a new thread). Best Regards, Andreas.
Part Number: TRF7962A Hi All,
I have a question about TRF7962A.
The customer has performed an electrostatic test on the TRF7962A. If static electricity enters the control line, the operation of the IC will freeze. It does not recover even if the reset bit…
Part Number: TRF7962A Hi,
My customers have a question about the crystal matching of TRF7962A. They are doing crystal matching test.
They tried C1 and C2 with two patterns, 22pF and 27pF.
In general, frequency will increase when the capacitance is small…
Part Number: TRF7962A Other Parts Discussed in Thread: TRF7964A , TRF7960A , TRF7970A Hello TI experts,
my customer considers TRF7962A for their new product now, they just drew 1st schematic.
and they have a problem with making NFC antenna, because it is…
Part Number: TRF7962A Hi, My customers have questions about the EN/EN2 pins of the TRF7962A.
Now customer's design is EN---VDD_X (1kΩ pull-up) EN2 ---GND (1kΩ pull-down)
Due to this connection, the IC may enter power-down mode and not work…
Part Number: TRF7962A M_Read Single Block.xlsx
To: TI Support Team
Customer has a problem of Read_Single_Block operation (ISO15693) with some TRF7962A ICs. If they swapped each IC, the a bad board became a good and a good board was a bad. Therefore, we…