Part Number: MSP-3P-SEARCH Other Parts Discussed in Thread: MSP430WARE Tool/software: MSP430 Virtual COM Port Driver file for WINDOWS OS with ARM processor.
Part Number: SAYKAL-3P-ALLINONE Tool/software: Hello,
I am trying to install CCS on Redhat Linux 8. It looks like there is a gcc dependency and it needs to be 3.3 which RHEL 8 does not.
Is there a version you can send me that is supported on Redhat…
Hello Zain,
Zain Alishammat said: And in the PDK API there are functions we can use to set this frequency.
You mention PDK API, can you point me to specifically what PDK?
Also, are you planning on using Linux OS?
Zain Alishammat said: There is…
Hi Saurav,
saurav pandya said: I am working to build for EVK (SK-AM62) using step from link ( https://software-dl.ti.com/processor-sdk-linux/esd/AM62X/08_06_00_42/exports/docs/linux/Overview_Building_the_SDK.html) and host system is ubuntu 20.04.
…
Part Number: OCTVO-3P-AM335X Hello Everyone,
I am new bie for yocto and i wan to create yocto image for Pocketbeagle, i dont know if it is possible or not if yes then provide me how can i build OS
Regards Prial
Rasty
I believe you have evaluated AM64 in the past , and had some critical feedback on performance for it to be a replacement for AM57x.
AM24 belongs to the same family - what pre-evaluation was done prior to picking this for your project, what are…
Per 7/21 call, Juergen provide position on call:
TI supports Linux a default OS. Any other HLOS migration is responsibility of customer and/or 3P working OS vendor
For TIDL-RT, TI continues to use very minimal OS features so any porting to any Posix…
Hi,
The PDK that is installed as part of PSDK RTOS, is used to create images for the R5 / C7x / C6x cores. As the PSDK RTOS PDK contains an OS abstraction layer (OSAL), it can also be used for other 3P HLOSs and/or for other cores, with minor modifications…
Hi Ashish,
I have tried to change this at my end and I see that the builds are happeneing fine when the CATEGORY is changed. Can you please update if you're using any other 3P OS's like vectorOS etc.,?
can you please post the entire error message…
Hello Vivek and Akshay,
Apologies for the delay in getting back, this seems to have slipped through the cracks.
Akshay Katare said: Could you please confirm, which SDK is better to use for the Autosar based environment whether Linux based or Windows…