Part Number: TS12A12511 Hi,
I want to use the TS12A12511DCNR in our PCB; Supply Voltage of the switch is 12V; the control signal for the switch (pin 6 "IN") is generated by an uC and is 4.5V. According the specificartion of the TS12A12511DCNR…
Part Number: TS12A12511 Hello,
I checked the data sheet of TS12A12511. For Digital inputs, the absolute maximum rating is It is not listed. Please tell me the range of absolute maximum ratings.
Best Regards, DDdoor
Part Number: TS12A12511 Other Parts Discussed in Thread: TINA-TI , Tool/software: TINA-TI or Spice Models The customer wants to simulate the TS12A12511 Peak current circuit. Can you provide a simulation model?
Part Number: TS12A12511 Other Parts Discussed in Thread: TPS2120 Hi,
I need a switch for my board design to toggle between USB and Battery,
- The board can be powered by USB(5V) or Battery(7.4V)
- When USB connected for programming, I need to remove battery…
Part Number: TS12A12511 Hello Adam,
one of my customer configured dual supply Vcc(+/-5V) schematic to get +/-4V swing output. COM should be output connected to load and NC, NO are applied from Vcc through resistor divider. IN comes from 0~3.3V 150Hz swing…
Part Number: TS12A12511 Other Parts Discussed in Thread: TS5A12301E Hello. I am considering using the TS12A12511, however, section 10 of the datasheet is giving me pause. That section indicates a requirement for sequencing VCC followed by NC, NO, and…
Part Number: TS12A12511 Other Parts Discussed in Thread: TS5A23160 , TS3A5223 , TS3A27518E hi dear supporting team,
there is one concern from customer on both TS12A12511 and SN74CBTLV3257DBQR, for an example, with A port and B port input, and output to COM…
Thayaparan,
You may use the PSPICE model for TS12A4517 for the TS12A4516 as well since they are so similar found on the tools and software tab .
To help me place a request from the modeling team for the TS12A12511 would you please provide which simulator…
Part Number: TS12A12511 My customer is asking for temperature drift data on the TS12A12511:
"I need to know how the resistance changes with temperature to see if it is stable enough for an analog signal in our scale."
He is looking for the…