Part Number: TS12A12511 I use TS12A12511 to modulate the voltage that sets the current (-2.5V - +2.5V). At the moment on NC and NO I have 0V. I noticed that my MCU was very warm. Seems I have -5V on my input IN. At the moment the open drain is on the MCU…
Part Number: TS12A12511 Other Parts Discussed in Thread: TMUX1072 Hi Experts:
Can I know the relative internal circuit of the pinout of COM, NC, IN, NO because my customer want to know the behavior of the scenario below ?
a) input 12V on the COM pin , and…
Kailyn,
I went and made a very crude board in the lab to double check the TS12A12511 bandwidth is close to the datasheet value.
The measurement below was taken from NO to COM with Vcc = 12V, V-=GND, and IN= 12 V. You can see the curve isn't very smooth…
Part Number: TS12A12511 I have a question.
When VCC = 10V. Please tell me about (MIN) of VINH.
Background of the question ======================
My customer using Vcc=10V, -VCC=GND.
And,IN=0V/3.3V.
They say that they are using it without problems.
===…
Part Number: TS12A12511
The customer is asking whether IN port of TS12A12511 can support 3.3V or not? According to the datasheet, it seems the IN port support only 5V, but could you tell me whether 3.3V is available on IN port, or not?
Part Number: TS12A12511 Hi Switches & Multiplexers team,
We're looking for an Analog Switch that will be used at the output of a couple audio amplifiers (two amplifiers, one speaker). One of the amplifiers will output voltage up to 8.5V. Looking…
Part Number: TS12A12511 Hi,
VCC_CATH can be between 0V to -2.4V referenced to GND.
VCATH_SW_EN is connected to a 3.3V GPIO referenced to GND.
I saw in a post that VIL and GND pins are internally connected in the IC.
Please see if the circuit functions…
Dino,
The current capability of the signal switches are listed in the absolute maximum ratings table. The TS12A12511 will handle up to 50mA.
The signal switches covered in this forum are low power switches typically 10-500 mA. I would recommend posting…
Part Number: TS12A12511 Other Parts Discussed in Thread: CD4053B Hello,
I'd like to know if we have a solution like TS12A12511 only with four channels (dual channels would be also acceptable)
The requirement is to work with negative signaling between…
Part Number: TS12A12511 Hi experts.
We met a strange issue with the application of TS12A12511DRJR. Submit a help thread before, but no finding, so we continue to debug it .
We use +5V , -5V power TS12A12511DRJR to pass -4 - -1 volt voltage. When we po…