Part Number: TS3A26746E Other Parts Discussed in Thread: TS5A22364 Hi Sirs, Would you pls advise that if the TS3A26746E suitable for de-pop noise application? Do we have application example or application note to address it? Thank you and Best regards, …
Other Parts Discussed in Thread: TS3A227E , TS3A225E , TS3A226AE In both 3.5mm audio jack and USB Type-C connectors the location of the mic and ground signals from the audio accessory may appear on different pins in the system. For the 3.5 mm jack accessores…
Part Number: TS3A26746E Hello team,
we are looking for a solution for splitting and mixing analog audio signals (voice transmission) for a configuration where 3 users can talk to each other.
Each of the users can call the master user, and master user…
Hi Sunny,
1. You must connect the tip pin of the TS3A226AE in order for them to properly execute the detection sequence. All our TI audio jacks switches use the TIP, Ring2, and Sleeve pins of the audio jack to do the detection.
2. However, if you want to…
TJ,
That is correct the headset will need to have the same ground path for the audio jack switch devices to make the impedance measurement which is the way it automatically locates the ground and mic nodes.
If you don't need the automatic detection of…
Other Parts Discussed in Thread: TS3A26746E , TS3DS10224 Hello,
Do we have a p2p alternative to the MAX4528: datasheets.maximintegrated.com/.../MAX4528.pdf
I didn't see anything like this in our portfolio. An alternative that I can think of is to tie the…
Hi Adam, I do not know how many bits you need to swap.
TS3A26746E can have 1-bit swap.
SN74CBTLV3383 can take up to 5-bit bus swap.
SN74CBT3383 can take up to 5-bit bus swap. And its supply is 5V.
Other Parts Discussed in Thread: TS3A26746E , TS3A227E Hi Expert,
I found the TI design for Type C audio solution, that used the TS3A227E swithc for microphone and GND. But some data used TS3A26746E. I have some question.
1. Which one is better?
2. Does…
Other Parts Discussed in Thread: TS3A227E , TS3A225E , TS3A226AE , TS3A26746E In the blog, USB Type-C audio: Do I need to buy a new pair of headphones?, the crosspoint switch TS3A26746E is mentioned as an alternative to the TS3A226AE which is used in the reference…
SHH,
We have 4 different audio jack switches that are similar to the FSA8039 and you can see more information about the differences in the thread below.
What is the difference between the 4 audio jack switches TS3A26746, TS3A225E, TS3A226AE, and TS3…