Part Number: TS5A22362 Other Parts Discussed in Thread: TS5A22366 , TMUX2889
Hi team,
The customer has a special application where they switch between audio signals and I2C signals on the audio jack, as shown in the diagram below.
But when switching to…
Part Number: TS5A22362 Other Parts Discussed in Thread: TPS60403 , CD74HC4053 Dear expert,
Input signal is +/-2.5V when in 3.3VCC application.
Based on recommendation operating condition, TS5A22362 cannot support this application. (3.3-5.5=-2.2V)
But…
Part Number: TS5A22362 Hi,
We attend to use TS5A22362DGSR and TS5A23159DGSR on our circuit. For supply voltage, they are applied to 3.3V and 5V respectively.
I have two questions below.
1. What the propagation delay for each?
2. I saw two parameters: ton…
Part Number: TS5A22362 Other Parts Discussed in Thread: TS3A24159 an engineer advised that this ADI switch in new design has very long lead times and is asking if TI has a P2P replacement for it.
(ADG884BRMZ-REEL7)
I see parts such as TS5A22362 are similar…
Part Number: TS5A22362 Hi TI expert,
If we want to use the TS5A22362 to switch the signal output from Codec to Headset & Speaker.
We shall connect the Codec part to COM1 & COM2 and the Audio Source 1 & 2(NC1/NC2 or NO1/NO2) will be the Headset and…
Part Number: TS5A22362 Other Parts Discussed in Thread: STRIKE Hi Team,
We would like to know detail measurement circuit of ON/OFF leakage current.
I understand it is the circuit below.
Is my understanding correct?
If no, could you please let us know…
Part Number: TS5A22362 e2e,
I want some clarification on the TS5A22362DRCR and TS5A22362DRCR-NM package drawings. There are two different package drawings with different dimensions, DRC and DRC0010J.
Which drawing corresponds to which magnetics status…
Part Number: TS5A22362 Dear team,
Customer want to know the status between pin COM1 and NC1? HIZ or ON? Or other status without power supply.
Thanks.
Best regards,
Sammi
Part Number: TS5A22362 I am using TS5A22362 for switching analog input Voltages applied to differential ADC. Supply for TS5A22362 is 3.3V. Input signal is from -450 mv to +450 mV.
I am facing problem when the input terminal (NC & NO) of TS5A22362 switch…