Part Number: TS5A22362 Hi TI experts,
I'm going to use this switch to direct continuous current (output from a power supply) to either one of the two loops. As attached.
Power supply will constantly output for example 1A current.
I have two concern…
Hi Ian,
Currently we do not have a signal switch in our portfolio that will conduct without power to the IC. You can try searching the web for a depletion FET switch but TI doesn't have one of these types of devices at this time.
Regards,
Samina…
Part Number: TS5A22362 I'm trying to allow a user to plug and unplug a series-connected differential serial device in and out of the circuit on the fly.
When the device is plugged in the "Board Device Present" is pulled to 5V by an externally supplied…
Hi Ian,
Yes, If you look at the block diagram for TS5A22362, you could use NC1 for SE and NO1 and NO2 as differential inputs. (Put NC2 to ground)
It is a good practice to ground unused input pins in the SE use case to avoid any undesirable signal reflections…
Part Number: TS5A22362
Hi TI experts, I'm trying to some circuit simulation to test the TS5A22362. I have the following questions:
1) Can the hspice model that provided on the website be imported into the Cadence PSPICE simulator? I was not able to…
Part Number: TS5A22362 Hi,
I'm writing to ask about the maximum current rating regarding the datasheet:
If I understand it correctly. Although this switch can handle the negative voltage, VNC, VNO, and VCOM all have to be positive (0 to Vcc) to have…
Part Number: TS5A22362
Hello E2E,
Need help to identify part that can be used to switch between a signal and power supply (SPDT-Single,Dual or Quad port - any). I see TS5A22362 can be used for upto 350mA with DBGA package but I am looking for more than…
Part Number: TS5A22362 Hi,
I'm writing to ask if there is a stencil for the part TS5A22362YZPR? Or is there a desktop stencil machine that can make a stencil for the PCB containing this part?
Thank you very much for your help.
Yixin Ma
Part Number: TS5A22362 Other Parts Discussed in Thread: TS5A22364 , Hi,
I need to have SPDT switches in my application. Previously I chose the TS5A22364 switch and got into a huge mess with my circuit because when the unconnected leg goes to ground via…