Part Number: TS5A22362 Hello team,
One of my customer is asking the top marking of TS5A22362
On datasheet, top marking of BGA type is 39392
However, my customer found that a device has ' 424392' on top
Could you check the whether TS5A22362 has…
Part Number: TS5A22362 Other Parts Discussed in Thread: TS5A22364 , Hi,
My customer is also urgently finding the package size of YZP, but the web information is unfortunately not fixed yet.
Also the related link mentioned in this previous E2E is even dead so…
Part Number: TS5A22362 Hi all
I need to use the switch in a medical application and can see that the IC has ESD protection. Is this enough or do I have to add some extra's?
Kind regards
Dries
Part Number: TS5A22364 Other Parts Discussed in Thread: TS5A22362 Hello team,
My customer would like to use TS5A22364 or TS5A22362 so they would like to know how "Negative Signaling Capability" features can be used with 2.3~5.5VCC and GND?
Please…
Part Number: TS5A22362 e2e,
In the recommended condition, VCC range is 2.3V to 5.5V and VIN max is saying 5.5V.
In a given scenario, VIN would be higher than VCC voltage, for example, VCC = 3.3V or 1.8V, but VIN = 5.5V.
Is this use case allowed combination…
Part Number: TS5A22362 Hi,
I am looking for clarification on the positioning of the A1 ball of the ts5a22362 device with respect to the package marking and dimensions.
In the different documents, the information is quite unclear.
Thanks for your help…
Part Number: TS5A22362 Other Parts Discussed in Thread: TS5A22366 e2e,
I have another question related to the TS5A22362 I was hoping you could help with.
The input logic high (min) is 1.4V for both 2.7 and 3.3V operation of the TS5A22362, but I wonder…
Other Parts Discussed in Thread: TS5A22362 , TS3A44159 Hi team,
For slow rising time issue like below figure when using TS5A22362 for SPI interface, can you give some analysis and the workaround for customer? Is there a part that will work better for this…
Part Number: TS5A22362 Other Parts Discussed in Thread: TS5A23159 End user send information to us that they test TS5A22362 COM is connect to NC or NO when the audio source hasn't power on.
I see the part doesn't suggest com folat and NC ,NO float…